package xdc.tools.check |
![](../../../Arrow_right.png) |
Check compatibility of specified packages
This tools scans the specified repositories looking for package
incompatibilities.
[
more ... ]
package xdc.tools.check [1, 0, 0] {
// Command implementation
}
USAGE
xs xdc.tools.check [--help]
[-[ax]] [-v] [-t target] [-e exclude_pattern] [-H header] [repository ...]
OPTIONS
- -a
- Return an array of strings
- -v
- Print informative messages during execution
- -x
- Return a Results struct as XML
- -H
- Prepend Header label to output
- -e
- Exclude packages or targets from checks
Do not check compatibility of packages or targets whose names match
the regular expression exclude.
- -m
- Allow checking multiple versions of the same package
By default, when a package appears in more than repository named on
the command line, this tool only checks the first occurance
of the package. Setting this option forces all versions of all
packages in the specified repositories to be included in the checks.
- -t
- Target to check
During the compatibility checks this tool ensures that for all
targets used by all packages are compatible with the latest target
referenced by any package. If this option is set, the check tool
will only validate compatibility for the specified target. In
addition, if the target string contains a target compatibility key,
all packages that reference the target will be checked for
compatibility with the specified key.
The format of this string is either
<target_name>:<target_key>
or
<target_name>
where <target_name> is the full name of a target and <target_key>
is an optional target-specific compatibility key. The optional
target compatibility key can be used to validate the set of packages
against a specific compiler tool chain.
DETAILS
This tools scans the specified repositories looking for package
incompatibilities.
By default, if a package appears in more than one repository, only the
package in the first repository is added to the set of packages to check.
This allows one to check the consistency of all packages that can be found
along a specified package path by simply listing the package path
repositories on the command line.
This tool performs the following checks:
- the latest version of each target used by any package is compatible
with all other versions used; and
- the "built-with" versions of all packages are compatible with the
versions of the packages contained in the specified repositories
If no repositories are specified, the repositories named in the current
package path are checked.
generated on Wed, 20 Jul 2011 20:33:37 GMT