1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Thread.xdc ========
15 */
16
17 import xdc.runtime.Error;
18 import xdc.runtime.Assert;
19 import xdc.runtime.knl.IThreadSupport;
20
21 /*!
22 * ======== Thread ========
23 * Thread services.
24 *
25 * This module manages threads through a proxy which inherits from
26 * IThreadSupport interface. It has a module wide config parameter
27 * {@link #Proxy} which needs to be bound to an OS specific delegate before
28 * this module can be used.
29 *
30 * Here is an example showing how the proxy is bound to a BIOS 6.x specific
31 * delegate.
32 *
33 * @p(code) 34 * var Thread = xdc.useModule('xdc.runtime.knl.Thread');
35 * Thread.Proxy = xdc.useModule('ti.sysbios.xdcruntime.ThreadSupport');
36 * @p 37 *
38 * Typically a package containing the delegates has a Settings module that
39 * will bind all {@link xdc.runtime.knl} proxies. The following
40 * example sets up all the xdc.runtime.knl proxies.
41 *
42 * @p(code) 43 * xdc.useModule('ti.sysbios.xdcruntime.Settings');
44 * @p 45 */
46
47 @InstanceInitError /* because initialization can fail */
48 @InstanceFinalize /* have to Thread_Proxy_delete(sem) on delete */
49
50 module Thread
51 {
52 /*! Thread priorities which are mapped to OS specific value by Proxy */
53 enum Priority {
54 Priority_INVALID,
55 Priority_LOWEST,
56 Priority_BELOW_NORMAL,
57 Priority_NORMAL,
58 Priority_ABOVE_NORMAL,
59 Priority_HIGHEST
60 };
61
62 /*! Invalid OS priority value */
63 const Int INVALID_OS_PRIORITY = 0;
64
65 /*! Status returned by {@link #getPri} when an error occurs */
66 const Int GETPRI_FAILED = -2;
67
68 /*! Status returned by {@link #compareOsPriorities} when an error occurs */
69 enum CompStatus {
70 CompStatus_ERROR = -2,
71 CompStatus_LOWER = -1,
72 CompStatus_EQUAL = 0,
73 CompStatus_HIGHER = 1
74 };
75
76 /*! Proxy that needs to be bound to an OS specific delegate. */
77 proxy Proxy inherits IThreadSupport;
78
79 /*! Typedef for thread function */
80 typedef Void (*RunFxn)(IArg);
81
82 /*! Struct to hold thread statistics from {@link #stat} */
83 struct Stat {
84 SizeT stackSize;
85 SizeT stackUsed;
86 }
87
88 /*! Assert when timeout passed to {@link #sleep} is zero */
89 config Assert.Id A_zeroTimeout= {
90 msg: "A_zeroTimeout: Timeout value annot be zero"
91 };
92
93 /*! Default thread stack size. */
94 config SizeT defaultStackSize = 0;
95
96 /*!
97 * ======== self ========
98 * Return the currently executing thread's handle
99 *
100 * @param(eb) Pointer to Error.Block
101 * @a(returns) Returns a handle to the currently executing thread.
102 * If the current thread is the main thread, this function
103 * returns `NULL`. NULL is also returned in case of error.
104 */
105 @DirectCall
106 Handle self(Error.Block *eb);
107
108 /*!
109 * ======== start ========
110 * Start threads running
111 *
112 * This function can be used to start all statically created threads,
113 * and all threads created dynamically before this function is called.
114 * Any thread created after this function is called, starts automatically.
115 * (i.e., there is no need to call Thread_start() more than once).
116 *
117 * @param(eb) Pointer to Error.Block
118 * @a(returns) true for success; false for error
119 */
120 Bool start(Error.Block *eb);
121
122 /*!
123 * ======== yield ========
124 * Yield the currently scheduled thread
125 *
126 * @param(eb) Pointer to Error.Block
127 * @a(returns) true for success; false for error
128 */
129 Bool yield(Error.Block *eb);
130
131 /*!
132 * ======== compareOsPriorities ========
133 * Compare two os specific priority values and find out which one
134 * represents a higher priority.
135 *
136 * @p(blist) 137 * -{@link #CompStatus_ERROR} if an error occured
138 * -{@link #CompStatus_LOWER} if p1 is lower than p2
139 * -{@link #CompStatus_EQUAL} if p1=p2
140 * -{@link #CompStatus_HIGHER} if p1 is higher than p2
141 * details.
142 * @p 143 *
144 * @param(p1) priority one
145 * @param(p2) priority two
146 * @param(eb) Pointer to Error.Block
147 * @a(returns) refer to description above
148 */
149 Int compareOsPriorities(Int p1, Int p2, Error.Block *eb);
150
151 /*!
152 * ======== sleep ========
153 * Sleep for given number of microseconds
154 *
155 * This function is gauranteed to sleep for at least as long as the
156 * timeout value but the actual sleep time may be longer. NOTE:
157 * The timeout value cannot be zero.
158 *
159 * @param(timeout) timeout in microseconds
160 * @param(eb) Pointer to Error.Block
161 * @a(returns) true for success; false for error
162 */
163 Bool sleep(UInt timeout, Error.Block *eb);
164
165 instance:
166
167 /*! Thread function argument. Default is 0. */
168 config IArg arg = 0;
169
170 /*!
171 * ======== priority ========
172 * Specify the new thread's priority
173 *
174 * Thread defines several constants which allows applications to select
175 * a priority in an OS independent way: Priority_LOWEST,
176 * Priority_BELOW_NORMAL, Priority_NORMAL, Priority_ABOVE_NORMAL and
177 * Priority_HIGHEST. These values get mapped to OS specific priorities
178 * by the OS specific delegate.
179 */
180 config Priority priority = Priority_NORMAL;
181
182 /*!
183 * ======== osPriority ========
184 * OS specific thread priority
185 *
186 * Used to specify an OS specific value for priority. If set this value
187 * takes precedence over {@link #priority}.
188 */
189 config Int osPriority = INVALID_OS_PRIORITY;
190
191 /*!
192 * ======== stackSize ========
193 * Thread stack size
194 *
195 * The default value of 0 means that `{@link #defaultStackSize}` is used.
196 */
197 config SizeT stackSize = 0;
198
199 /*!
200 * ======== tls ========
201 * Thread local storage.
202 *
203 * User data associated with a thread. Must persist for the life of
204 * the thread.
205 */
206 config Ptr tls = null;
207
208 /*!
209 * ======== create ========
210 * Create a Thread object
211 *
212 * This function spawns a new thread calling the function fxn.
213 *
214 * @param(fxn) function for new thread to begin execution
215 */
216 create(RunFxn fxn);
217
218 /*!
219 * ======== join ========
220 * Block calling thread until given thread terminates.
221 *
222 * Use this functions to ensure that a thread has terminated. It is OK to
223 * call this function on a thread that has already terminated.
224 *
225 * @param(eb) Pointer to Error.Block
226 * @a(returns) true for success; false for error
227 */
228 Bool join(Error.Block *eb);
229
230 /*!
231 * ======== getPriority ========
232 * Obtain a thread's priority.
233 *
234 * For OSes that support dynamic priority boosting, this function
235 * retrieves the base priority of the thread.
236 *
237 * @param(eb) Pointer to Error.Block
238 * @a(returns) thread priority in case of success; PRIORITY_INVALID in
239 * case of error;
240 */
241 Priority getPriority(Error.Block *eb);
242
243 /*!
244 * ======== setPriority ========
245 * Set a thread's priority.
246 *
247 * For OSes that support dynamic priority boosting, this function
248 * changes the base priority of the thread.
249 *
250 * @param(newPri) new thread priority
251 * @param(eb) Pointer to Error.Block
252 * @a(returns) true for success; false for error
253 */
254 Bool setPriority(Priority newPri, Error.Block *eb);
255
256 /*!
257 * ======== getOsPriority ========
258 * Obtain a thread's OS specific priority.
259 *
260 * For OSes that support dynamic priority boosting, the value returned
261 * is the base priority of the thread.
262 *
263 * @param(eb) Pointer to Error.Block
264 * @a(returns) thread priority in case of success; GETPRI_FAILED in
265 * case of error;
266 */
267 Int getOsPriority(Error.Block *eb);
268
269 /*!
270 * ======== setOsPriority ========
271 * Set a thread's priority.
272 *
273 * This API sets the base priority of the thread on OSes that
274 * support dynamic priority boosting
275 *
276 * @param(newPri) new thread priority
277 * @param(eb) Pointer to Error.Block
278 * @a(returns) true for success; false for error
279 */
280 Bool setOsPriority(Int newPri, Error.Block *eb);
281
282 /*!
283 * ======== getOsHandle ========
284 * Get the OS thread handle
285 *
286 * @a(returns) OS thread handle
287 */
288 Ptr getOsHandle();
289
290 /*!
291 * ======== getTls ========
292 * Obtain a thread's local storage.
293 *
294 * @a(returns) null when tls has not been set.
295 */
296 Ptr getTls();
297
298 /*!
299 * ======== setTls ========
300 * Change a thread's local storage.
301 *
302 * @param(tls) tls
303 */
304 Void setTls(Ptr tls);
305
306 /*!
307 * ======== stat ========
308 * Get thread statistics
309 *
310 * @param(buf) Pointer to Stat
311 * @param(eb) Pointer to Error.Block
312 * @a(returns) true for success; false for failure
313 */
314 Bool stat(Stat* buf, Error.Block *eb);
315
316 internal:
317
318 struct Instance_State {
319 Thread.Proxy.Handle proxyHandle; /*! handle for real implementation */
320 Ptr tls; /*! store tls parameter */
321 }
322 }
323 /*
324 * @(#) xdc.runtime.knl; 1, 0, 0,148; 7-14-2011 17:22:15; /db/ztree/library/trees/xdc/xdc-x16x/src/packages/
325 */
326