package ti.platforms.evm6670 |
|
Platform package for the 6670 EVM
This package implements the interfaces (xdc.platform.IPlatform)
[
more ... ]
package ti.platforms.evm6670 [1, 0, 0, 0] {
// Platform support for the evm6670
}
DETAILS
This package implements the interfaces (xdc.platform.IPlatform)
THROWS
XDCException exceptions are thrown for fatal errors. The following error
codes are reported in the exception message:
- ti.platfoms.evm6670.LINK_TEMPLATE_ERROR
-
This error is raised when this platform cannot found the default
linker command template linkcmd.xdt in the build target's
package. When a target does not contain this file, the config
parameter xdc.cfg.Program.linkTemplate must be set.
generated on Wed, 20 Jul 2011 20:36:15 GMT