1 /*
2 * Copyright (c) 2009 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== ITarget.xdc ========
14 *
15 */
16
17 /*!
18 * ======== ITarget ========
19 * A TI specific extension to the base `xdc.bld.ITarget2` interface.
20 */
21 @TargetHeader("xdc/bld/stddefs.xdt")
22 metaonlyinterface ITarget inherits xdc.bld.ITarget2 {
23
24 overridereadonlyconfig string stdInclude = "ti/targets/std.h";
25
26 /*!
27 * ======== binDir ========
28 * This parameter controls the location of the target's commands.
29 *
30 * All build commands returned within a command set
31 * (`xdc.bld.ITarget.CommandSet.cmds`) are formed by prefixing `binDir`
32 * to this target's Command.cmd specification. For example, the
33 * compile command returned is formed as follows:
34 * @p(code) 35 * $(binDir)$(cc.cmd)
36 * @p 37 * where, `$(binDir)` is this target's `binDir` value and `$(cc.cmd)` is
38 * the value of this target's `cc.cmd` string.
39 *
40 * If `binDir` is non-empty then it must end with '/'. If it is empty,
41 * the target's commands (compiler, linker, archiver, etc.) will be
42 * located along a path constructed from this target's `pathPrefix`.
43 */
44 config string binDir = "$(rootDir)/bin/";
45
46 /*!
47 * ======== pathPrefix ========
48 * A prefix to the PATH environment variable
49 *
50 * Each target command is executed with C_DIR set to "" and PATH
51 * set as follows:
52 * @p(code) 53 * $(pathPrefix);$(binDir);$(PATH)
54 * @p 55 * where, `$(pathPrefix)` and `$(binDir)` are the values of the
56 * configuration parameters and `$(PATH)` is the value of the `PATH`
57 * environment variable set by the `xdc` command (type 'xdc -n' to
58 * see this).
59 *
60 * Embedded ';' characters within `pathPrefix` separate directory
61 * names. On UNIX hosts these ';' characters are convered to an
62 * appropriate separator; i.e., ':'.
63 */
64 config string pathPrefix = "";
65
66 overrideconfig String binaryParser = "ti.targets.omf.cof.Coff";
67
68 /*!
69 * ======== debugGen ========
70 * TI Debugger/IDE file generation support.
71 *
72 * The settings below generate CCS project files that enable one
73 * to debug (and even rebuild) Executables from within the CCS GUI.
74 *
75 * To avoid unnecessary build time overhead, these files are not always
76 * generated; by default, they are only generated for "debug" profiles.
77 * The generation of these files is controlled by the
78 * `{@link xdc.cfg.Program#gen}` configuration parameter. To force these
79 * files to be generated for a particular executable, add the following
80 * line to the executable's program configuration script:
81 * @p(code) 82 * Program.gen.debuggerFiles = true;
83 * @p 84 * It is also possible to control the generation via build options; see
85 * `{@link xdc.bld.ITarget#DebugGen}`.
86 *
87 * Note: if you are using CCS 2.x, disable CodeMaestro to prevent
88 * instabilities when re-loading project files. CodeMaestro can be
89 * disabled via: Options->"Customize ..."->"CodeMaestro Settings"
90 *
91 * To debug an executable:
92 * @p(nlist) 93 * - load generated project for the executable:
94 * package/cfg/<cfg_name>.pjt
95 * - load generated GEL script for the executable:
96 * package/cfg/<cfg_name>.gel
97 * - load prerequisite packages:
98 * GEL->"XDC Package"->open_project
99 * @p 100 * where <cfg_name> is the name of the executable (foo.x62) with the
101 * '.' replaced by and '_' (foo_x62).
102 *
103 * Alternatively, one can use the `ccs_start.pl` script in this package
104 * to automate the steps above. In addition, it is possible to
105 * associate `ccs_start.bat` (also in this package) with the generated
106 * `.pjt` files to automate the above by double-clicking on the `.pjt`
107 * file.
108 *
109 * To avoid navigation to the executable via file menus, you can load
110 * the executable associated with the project via:
111 *
112 * GEL->"XDC Package"->load_executable
113 *
114 * @a(See Also) `xdc.bld.ITarget` contains addition information about
115 * how to create and use these templates.
116 */
117 overrideconfig xdc.bld.ITarget.DebugGen debugGen = {
118 execTemplate : "ti/targets/ccs_exec.xdt",
119 execPattern : "$(cfgDir)$(cfgName).pjt",
120 packageTemplate: "ti/targets/ccs_package.xdt",
121 packagePattern : "package/$(pkgName).pjt"
122 };
123
124 /*!
125 * ======== extensions ========
126 * File extensions recognized by TI targets
127 *
128 * @a(TI Specifics) 129 * For TI targets, the `typ` string field of an
130 * `xdc.bld.ITarget.Extension` structure may be of the form
131 * `"<cmd>:<langOpt>"` where `<cmd>` is one of `"asm"`, `"c"`, `"cpp"`,
132 * and `<langOpt>` is the language option to used to identify the source
133 * language of a source file. This allows one to explicitly control the
134 * language flag passed to the compiler based on a source file's
135 * extension; in particular, one can define separate source extensions
136 * for "linear" and "scheduled" assembly files, or simply cause `".s62"`
137 * files to be treated as "linear" assembly rather than "scheduled"
138 * assembly.
139 *
140 * For example,
141 * @p(code) 142 * tiTargets.C62.extensions[".s62"] = {suf: ".s62", typ: "asm:-fl"};
143 * @p 144 * causes all `".s62"` files to be treated as linear assembly.
145 *
146 * If no ':' appears in the `typ` string, a default will be used:
147 * `"-fa"` for `"asm"` files `"-fc"` for `"c"` files, and `"-fp"` for
148 * `"cpp"` files.
149 */
150 overrideconfig xdc.bld.ITarget.Extension extensions[string] =
151 xdc.bld.ITarget.extensions;
152
153 /*!
154 * ======== profiles ========
155 * Standard options profiles for the TI tool-chain.
156 */
157 overrideconfig xdc.bld.ITarget.OptionSet profiles[string] = [
158 ["debug", {
159 compileOpts: {
160 copts: "-g",
161 defs: "-D_DEBUG_=1",
162 }
163 }],
164 ["release", {
165 compileOpts: {
166 copts: "-O2",
167 },
168 }],
169 ["profile", {
170 compileOpts: {
171 copts: "-gp",
172 },
173 }],
174 ["coverage", {
175 compileOpts: {
176 copts: "-gp",
177 },
178 }],
179 ["whole_program", {
180 compileOpts: {
181 copts: "-oe -O2 -mo",
182 },
183 }],
184 ["whole_program_debug", {
185 compileOpts: {
186 copts: "-oe --symdebug:dwarf -mo",
187 },
188 }],
189 ];
190
191 /*!
192 * ======== versionMap ========
193 * Map of TI compiler version numbers to compatibility keys.
194 *
195 * This map translates version string information from the compiler
196 * into a compatibility key. The compatibility key is used to validate
197 * consistency among a collection of packages used in a configuration.
198 *
199 * TI compiler strings are formed by parsing the output of the
200 * compiler's --compiler_revision option and creating a string of the
201 * form:
202 * @p(code) 203 * <comp>_<ver>
204 * @p 205 * where `<comp>` is the first word of the output and `<ver>` is the
206 * version number that appears on this same line.
207 *
208 * There are two forms of version numbers output by the TI code gen
209 * tools; an "old" style that is of the form "<major>.<minor>" and a
210 * new style of the form "<major>.<minor>.<update>[.<branch>][<qual>],
211 * where <major>, <minor>, <update>, and <branch> are non-negative
212 * integers and <qual> is of the form "[IBAP]<yyddd>", and <yyddd>
213 * is the last two digits of the year concatenated with the number of
214 * the day.
215 *
216 * If a compiler version is not found in this map the default is
217 * "1,0,<major>.<minor>" for old style version numbers, and
218 * "1,0,<major>.<minor>,<update>[.<branch>][,<yyddd>]" for new style
219 * version numbers.
220 *
221 * The user only needs to extend this table when a significant
222 * incompatibility occurs (and this package doesn't know about it) or
223 * when two versions of the compiler should be treated as 100%
224 * compatible.
225 *
226 * @a(Examples) 227 * @p(code) 228 * var C62 = xdc.useModule('ti.targets.C62');
229 *
230 * // assert that 4.0 is forward compatible with 4.32
231 * C62.versionMap["TMS320C6x_4.32"] = "1,0,4.0,0";
232 *
233 * // assert that 4.28 is incompatible with all other compilers
234 * C62.versionMap["TMS320C6x_4.28"] = "1,1,4.28,0";
235 */
236 overrideconfig string versionMap[string] = [
237 ["TMS320C6x_4.32", "1,0,4.32,0"],
238 ["TMS320C55x_2.56", "1,0,2.56,0"],
239 ["TMS320C54x_3.83", "1,0,3.83,0"],
240 ["TMS320C2000_3.07", "1,0,3.07,0"],
241 ];
242
243 /*!
244 * ======== alignDirectiveSupported ========
245 * The compiler supports an align directive.
246 */
247 overridereadonlyconfig Bool alignDirectiveSupported = true;
248
249 /*!
250 * ======== ccConfigOpts ========
251 * User configurable compiler options for the generated config C file.
252 */
253 overrideconfig xdc.bld.ITarget2.Options ccConfigOpts = {
254 prefix: "$(ccOpts.prefix) -mo",
255 suffix: "$(ccOpts.suffix)"
256 };
257
258 /*!
259 * ======== asmName ========
260 * The function that converts a C name into an assembly name
261 */
262 String asmName(String CName);
263
264 /*!
265 * ======== vers ========
266 * The command used to get the tool-chain to return a version number.
267 */
268 readonlyconfig xdc.bld.ITarget2.Command vers;
269
270 /*!
271 * ======== version ========
272 * The Compatibility Key associated with this target.
273 *
274 * The first two components of this target Compatibility Key are '1,0'.
275 * The rest of the Key represents the compiler version. The third
276 * component combines the major and the minor version number in the format
277 * Major.Minor. The fourth component is the patch number, and the optional
278 * fifth component is the version of an Alpha or Beta release.
279 *
280 * @a(Example) 281 * If this target's `rootDir` points to the compiler version 6.0.11, the
282 * Compatibility Key is [1,0,6.0,11]. If this target's `rootDir` points to
283 * the compiler version 7.0.0B1, the Compatibility Key is [1,0,7.0,0,1].
284 *
285 */
286 overridemetaonlyconfig String version;
287 }
288 /*
289 * @(#) ti.targets; 1, 0, 3,456; 6-9-2011 11:02:26; /db/ztree/library/trees/xdctargets/xdctargets-e05x/src/ xlibrary
290 291 */
292