1 /*
2 *Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*!
13 * ======== Main.xdc ========
14 * Check compatibility of specified packages
15 *
16 * This tools scans the specified repositories looking for package
17 * incompatibilities.
18 *
19 * By default, if a package appears in more than one repository, only the
20 * package in the first repository is added to the set of packages to check.
21 * This allows one to check the consistency of all packages that can be found
22 * along a specified package path by simply listing the package path
23 * repositories on the command line.
24 *
25 * This tool performs the following checks:
26 * @p(blist) 27 * - the latest version of each target used by any package is compatible
28 * with all other versions used; and
29 * - the "built-with" versions of all packages are compatible with the
30 * versions of the packages contained in the specified repositories
31 * @p 32 *
33 * If no repositories are specified, the repositories named in the current
34 * package path are checked.
35 */
36 metaonlymodule Main inherits xdc.tools.ICmd {
37
38 /*!
39 * ======== usage ========
40 * Usage message
41 */
42 overrideconfig String usage[] = [
43 '[-[ax]] [-v] [-t target] [-e exclude_pattern] [-H header] [repository ...]',
44 ];
45
46 /*!
47 * ======== Results ========
48 * XML output format
49 *
50 * This structure defines the "schema" for the XML output.
51 */
52 @XmlDtd
53 struct Results {
54 String header; /*! user specified header */
55 String errors[]; /*! array of all errors detected */
56 String warnings[]; /*! array of all warnings detected */
57 Target targets[];
58 }
59 struct Target {
60 String name; /*! target name */
61 struct {
62 String key; /*! target compatibility key used */
63 String packages[]; /*! all packages using target with this key */
64 } keys[];
65 }
66
67 instance:
68
69 /*!
70 * ======== arrFlag ========
71 * Return an array of strings
72 */
73 @CommandOption('a')
74 config Bool arrFlag = false;
75
76 /*!
77 * ======== verboseFlag ========
78 * Print informative messages during execution
79 */
80 @CommandOption('v')
81 config Bool verboseFlag = false;
82
83 /*!
84 * ======== xmlFlag ========
85 * Return a Results struct as XML
86 */
87 @CommandOption('x')
88 config Bool xmlFlag = false;
89
90 /*!
91 * ======== header ========
92 * Prepend Header label to output
93 */
94 @CommandOption('H')
95 config String header = null;
96
97 /*!
98 * ======== exclude ========
99 * Exclude packages or targets from checks
100 *
101 * Do not check compatibility of packages or targets whose names match
102 * the regular expression `exclude`.
103 */
104 @CommandOption('e')
105 config String exclude = null;
106
107 /*!
108 * ======== multipleFlag ========
109 * Allow checking multiple versions of the same package
110 *
111 * By default, when a package appears in more than repository named on
112 * the command line, this tool only checks the first occurance
113 * of the package. Setting this option forces all versions of all
114 * packages in the specified repositories to be included in the checks.
115 */
116 @CommandOption('m')
117 config Bool multipleFlag = false;
118
119 /*!
120 * ======== target ========
121 * Target to check
122 *
123 * During the compatibility checks this tool ensures that for all
124 * targets used by all packages are compatible with the latest target
125 * referenced by any package. If this option is set, the check tool
126 * will only validate compatibility for the specified target. In
127 * addition, if the target string contains a target compatibility key,
128 * all packages that reference the target will be checked for
129 * compatibility with the specified key.
130 *
131 * The format of this string is either
132 * @p(code) 133 * <target_name>:<target_key>
134 * @p 135 * or
136 * @p(code) 137 * <target_name>
138 * @p 139 * where `<target_name>` is the full name of a target and `<target_key>`
140 * is an optional target-specific compatibility key. The optional
141 * target compatibility key can be used to validate the set of packages
142 * against a specific compiler tool chain.
143 */
144 @CommandOption('t')
145 config String target = null;
146 }
147 /*
148 * @(#) xdc.tools.check; 1, 0, 0,206; 4-27-2011 15:33:00; /db/ztree/library/trees/xdctools/xdctools-e14x/src/
149 */
150