1 /*
2 * ======== Rta.xdc ========
3 */
4
5 package xdc.runtime;
6
7 /*!
8 * ======== Rta ========
9 * The Rta module contains target and configuration code for providing RTA
10 * support.
11 *
12 * The 'Command' enum defines the available control commands, and the
13 * 'CommandPacket' structure defines the format of commands received from
14 * the host.
15 *
16 * All commands should send back a response, even if only to acknowledge
17 * receipt and completion of the command. The format of the response
18 * is defined by the 'ResponsePacket' structure.
19 *
20 * The Rta_processCommand can be used to process commands received from a
21 * host to call the appropriate API. Alternatively, the individual APIs can
22 * be called if not all of the defined commands are used.
23 */
24 module Rta {
25
26 /*! Logged when the Agent receives a command */
27 config Log.Event LD_cmdRcvd = {
28 mask: Diags.USER2,
29 msg: "LD_cmdRcvd: Received command: %d, arg0: 0x%x, arg1: 0x%x"
30 };
31
32 /*! Logged when a diags mask is changed */
33 config Log.Event LD_writeMask = {
34 mask: Diags.USER2,
35 msg: "LD_writeMask: Mask addres: 0x%x, New mask value: 0x%x"
36 };
37
38 /*! Assert if logger id in control command is invalid. */
39 config Assert.Id A_invalidLogger = {
40 msg: "A_invalidLogger: The logger id %d is invalid."
41 };
42
43 /*! Error raised if Agent receives an invalid command. */
44 config Error.Id E_badCommand = {
45 msg: "E_badCommand: Received invalid command, id: %d."
46 };
47
48 /*! Command ids */
49 enum Command : Int {
50 Command_READ_MASK = 0,
51 Command_WRITE_MASK = 1,
52 Command_LOGGER_OFF = 2,
53 Command_LOGGER_ON = 3,
54 Command_GET_CPU_SPEED = 4,
55 Command_RESET_LOGGER = 5,
56 Command_CHANGE_PERIOD = 6,
57 Command_START_TX = 7,
58 Command_STOP_TX = 8
59 };
60
61 /*!
62 * Structure of command received from host
63 * TODO - Either the types should be changed to 32-bits, or the packet
64 * size information should be added to the RTA XML file.
65 */
66 struct CommandPacket {
67 Command cmdId;
68 UArg arg0;
69 UArg arg1;
70 }
71
72 /*! Structure of response packet sent back to host */
73 struct ResponsePacket {
74 Command cmdId;
75 UArg resp0;
76 UArg resp1;
77 }
78
79 /*!
80 * ======== dataTransportClassName =========
81 * The name of the xdc.rta.IDataTransport class to use.
82 *
83 * The class specified here can be used on the host for reading RTA data
84 * from this target application.
85 */
86 config String dataTransportClassName = "";
87
88 /*!
89 * ======== controlTransportClassName ========
90 * The name of the xdc.rta.IControlTransport class to use.
91 *
92 * The class specified here can be used on the host for communicating with
93 * this target application to send control commands and receive responses.
94 */
95 config String controlTransportClassName = "";
96
97 /*!
98 * ======== processCommand ========
99 * Executes a command packet and prepares the response packet.
100 *
101 * This API will execute the command specified by the command packet
102 * argument, and will store the response information in the response
103 * packet argument.
104 *
105 * @param(cmd) The CommandPacket to execute.
106 * @param(resp) The ResponsePacket to populate with the response.
107 */
108 Void processCommand(CommandPacket *cmd, ResponsePacket *resp);
109
110 /*!
111 * ======== acknowledgeCmd ========
112 */
113 Void acknowledgeCmd(ResponsePacket *resp);
114
115 /*!
116 * ======== readMask ========
117 */
118 Void readMask(ResponsePacket *resp, UArg addr);
119
120 /*!
121 * ======== writeMask ========
122 */
123 Void writeMask(ResponsePacket *resp, UArg addr, UArg val);
124
125 /*!
126 * ======== enableLog ========
127 */
128 Void enableLog(ResponsePacket *resp, UArg log);
129
130 /*!
131 * ======== disableLog ========
132 */
133 Void disableLog(ResponsePacket *resp, UArg log);
134
135 /*!
136 * ======== getCpuSpeed ========
137 */
138 Void getCpuSpeed(ResponsePacket *resp);
139
140 /*!
141 * ======== resetLog ========
142 */
143 Void resetLog(ResponsePacket *resp, UArg log);
144
145 /*!
146 * ======== changePeriod ========
147 */
148 Void changePeriod(ResponsePacket *resp, UArg period);
149
150 /*!
151 * @_nodoc 152 * ======== genRta ========
153 * Generates the Rta XML file.
154 */
155 function genRta(outputFileName);
156
157 }
158 /*
159 * @(#) xdc.runtime; 2, 1, 0,324; 4-29-2011 10:51:58; /db/ztree/library/trees/xdc/xdc-x03x/src/packages/
160 */
161