1 /*! 2 * ======== Main ======== 3 * Tool for reading and decoding RTA data from a file. 4 */ 5 metaonly module Main inherits xdc.tools.ICmd { 6 7 override config String usage[] = [ 8 ' ', 9 'Usage', 10 '[-p] [-h] [-m] [-e executable] [-x RTA XML file] [-d data input file] [-o output text file] [-c delimter character]', 11 '[--help]', 12 ' ', 13 ]; 14 15 instance: 16 17 /*! 18 * ======== printToScreen ======== 19 * Whether to print the decoded records to the console. 20 * 21 * You may use this tool to simply print the decoded records, or you 22 * may have them redirected to a file to be processed elsewhere. 23 */ 24 @CommandOption('p') 25 config Bool printToScreen = false; 26 27 /*! 28 * ======== suppressHeader ======== 29 * Don't print the header when printing the decoded records. 30 */ 31 @CommandOption('h') 32 config Bool suppressHeader = false; 33 34 /*! 35 * ======== more ======== 36 * Wait for the user to press enter before displaying the next packet. 37 * 38 * Without this flag, the tool will simply print all of the records in the 39 * data file to the screen. If this flag is set, then the tool will wait 40 * the user to press enter in between displaying each packet. 41 */ 42 @CommandOption('m') 43 config Bool more = false; 44 45 /*! 46 * ======== executable ======== 47 * Path to the executable which was used to generate the data file. 48 */ 49 @CommandOption('e') 50 config String executable = ""; 51 52 /*! 53 * ======== rtaXml ======== 54 * Optional path to the RTA XML file. 55 */ 56 @CommandOption('x') 57 config String rtaXml = ""; 58 59 /*! 60 * ======== dataFile ======== 61 * Path to the file containing the RTA log data. 62 */ 63 @CommandOption('d') 64 config String dataFile = ""; 65 66 /*! 67 * ======== outputFile ======== 68 * Optional path to an output file to write the decoded records to. 69 * 70 * The tool will write the decoded records out as text to the specified 71 * out file. The record properties will be separated with a delimeter 72 * character so that they can be imported into a spreadsheet such as 73 * Excel. 74 */ 75 @CommandOption('o') 76 config String outputFile = ""; 77 78 /*! 79 * ======== loadFile ======== 80 * // TODO 81 * [-l output file for load data] 82 */ 83 84 /*! 85 * ======== delimiter ======== 86 * Delimiter character to use when writing out the file. 87 * 88 * The character specified here will be inserted between each of the 89 * record fields so that the file can be imported into a spreadsheet 90 * such as excel. 91 */ 92 @CommandOption('c') 93 config String delimiter = "|"; 94 95 }