From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - Module-Object.PARAMS
Module's default instance creation parameters
Contents |
Synopsis
| «Mod».PARAMS; |
Description
For a module «Mod» that manage instances, «Mod».PARAMS is a "structure" that contains fields for each instance configuration parameter declared by «Mod» whose value is the default declared in the module's .xdc specification. This structure is identical to the value returned by creating a new «Mod».Params structure.
See also
XDCscript - Module-Object.create | Create a new Instance object managed by this unit |
XDCscript - Module-Object.Params | Module's instance creation parameters |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved