1    /*
     2     *  Copyright 2010 by Texas Instruments Incorporated.
     3     *
     4     */
     5    
     6    /*!
     7     *  ======== Main ========
     8     *  Command-line tool for generating eclipse plugins for RTSC content
     9     *
    10     *  The `plugingen` tool allows RTSC content producers to
    11     *  create eclipse plugins that allows their content to be 
    12     *  integrated in the CCS4 environment. As input, the tool requires 
    13     *  @p(blist)
    14     *      - a RTSC module implementing {@link xdc.tools.product.IProduct}
    15     *  @p
    16     *  Refer to {@link ./doc-files/ExampleProduct.xdc ExampleProduct}
    17     *  for an implementation of {@link xdc.tools.product.IProduct IProduct}.
    18     *
    19     *  The tool may also be used to generate starter examples that will showup 
    20     *  in the new project wizard. This is accomplished by implementing
    21     *  {@link xdc.tools.product.IProductTemplate IProductTemplate} and setting
    22     *  the {@link xdc.tools.product.IProduct#templateModule templateModule} 
    23     *  configuration parameter of the {@link xdc.tools.product.IProduct IProduct} 
    24     *  implementation to the name of the implementation module. 
    25     *  Refer to {@link ./doc-files/Examples.xdc Examples}
    26     *  for a sample implementation of {@link
    27     *  xdc.tools.product.IProductTemplate IProductTemplate}.
    28     *  
    29     *  The XGCONF product view maybe developed by implementing
    30     *  {@link xdc.tools.product.IProductView IProductView} and setting
    31     *  the {@link xdc.tools.product.IProduct#productViewModule productViewModule} 
    32     *  configuration parameter of the {@link xdc.tools.product.IProduct IProduct} 
    33     *  implementation to the name of the implementation module.
    34     *  Refer to {@link ./doc-files/ProductView.xdc ProductView.xdc} and 
    35     *  {@link ./doc-files/ProductView.xs ProductView.xs}
    36     *  for a sample implementation of {@link
    37     *  xdc.tools.product.IProductView IProductView}.
    38     *
    39     *  The tool operates on a product that is either specified by the `-p`
    40     *  option or is present in the folder from which the tool is executed.
    41     *  The tool will create the plugin in a sub-folder named `eclipse`
    42     *  in the output directory specified with `-o` option. If the `-o`
    43     *  option is not specified the plugin is created in the product root
    44     *  directory. 
    45     *  The tool will search the repositories specified in the module
    46     *  implementing {@link xdc.tools.product.IProduct} for RTSC platforms.
    47     *  This search can be disabled by specifying the`--disable_repo_search` 
    48     *  option. The user needs to ensure that the repositories are installed 
    49     *  in the product root directory before using the tool.
    50     *
    51     *
    52     *
    53     *  @a(Example)
    54     *  @p(code)
    55     *  xs xdc.tools.product.plugingen 
    56     *                      -p exampleprod_1_0_0_00
    57     *                      -m xdc.tools.product.plugingen.examples.ExampleProduct
    58     
    59     *
    60     */
    61    metaonly module Main inherits xdc.tools.ICmd
    62    {
    63        override config String usage[] = [
    64            '[-p product_root_directory]',
    65            ' -m module',
    66            '[-o outdir]',
    67            '[--suppress_product_type_info]',
    68            '[--disable_repo_search]'
    69        ];
    70    
    71    instance:
    72    
    73        /*!
    74         *  ======== productDir ========
    75         *  Product root directory
    76         *
    77         *  This option names the product root directory that is used by the 
    78         *  tool to generate the plugin. If the '-o' option is not
    79         *  specified the tool generates the plugin in a sub-directory
    80         *  called `eclipse` in the product root directory.
    81         *
    82         */
    83        @CommandOption("p")
    84        config String productDir = "./";
    85    
    86        /*!
    87         *  ======== schemaFile ========
    88         *  Input description of the plug-in to be specified
    89         *
    90         *  This required option names a module that implements
    91         *  `{@link xdc.tools.product.IProduct}`.
    92         *
    93         */
    94        @CommandOption("m")
    95        config String productModule;
    96    
    97        /*!
    98         *  ======== outputDir ========
    99         *  Output directory in which the plugin will be generated.
   100         *
   101         *  This option names the directory in which the plugin 
   102         *  will be generated in a sub-directory named `eclipse`.
   103         *  If this option is not specified the tool will generate
   104         *  the plugin in the product root directory specified with
   105         *  the '-p' option.
   106         *
   107         */
   108        @CommandOption("o")
   109        config String outputDir = null;
   110    
   111        /*!
   112         *  ======== suppress_product_type_info ========
   113         *  Suppress generation of product type information in the 
   114         *  generated plugin
   115         *
   116         * This option generates eclipse plugin without the product
   117         * type information. Should be invoked to generate plugins whose
   118         * product type is declared elsewhere 
   119         *
   120         */
   121        @CommandOption("suppress_product_type_info")
   122        config Bool suppressProductTypeInfo = false;
   123    
   124    
   125        /*!
   126         *  ======== disable_repo_search ========
   127         *  Suppress search of product repositories
   128         *
   129         *  If this option is specified the tool does not
   130         *  search the product repositories for RTSC platforms.
   131         */
   132        @CommandOption("disable_repo_search")
   133        config Bool suppressSearch = false;
   134    
   135            
   136        /*!
   137         *  ======== run ========
   138         */
   139        override Any run(xdc.tools.Cmdr.Instance cmdr, String args[]);
   140    }
   141    /*
   142     *  @(#) xdc.tools.product.plugingen; 1, 0, 0,39; 10-15-2010 11:41:40; /db/ztree/library/trees/xdctools/xdctools-d45x/src/
   143     */
   144