package xdc.shelf    

Container for third party jars required by XDCtools

The following jars are part of this package: [ more ... ]
XDCspec declarations sourced in xdc/shelf/package.xdc
package xdc.shelf [1, 0, 0] {
 
}
DETAILS
The following jars are part of this package:
Jar Version License From Description
js.jar 1.6R6 MPL 1.1 (note) http://www.mozilla.org/rhino Java implementation of JavaScript 1.5
xbean.jar 1.0.4 Apache 2.0 (note) http://svn.apache.org/repos/asf/xmlbeans/tags/1.0.4 XML support for JavaScript's E4X capabilities
jsr173_api.jar 1.0.1 Apache 2.0 http://dist.codehaus.org/stax/distributions/stax-src-1.2.0.zip JSR173 support required by xmlbeans
antlr.jar 3.1.1 BSD http://www.antlr.org LR parser generator used to implement the RTSC IDL
tar.jar 2.5 Public Domain http://www.trustice.com/java/tar tar file reader
In addition to the jars above, XDCtools requires the following third-party software:
Name Version License From Description
gmake 3.81 GPL v2 http://savannah.gnu.org/projects/make command run by the `xdc` command to create and build packages
J2SE Runtime Environment(JRE) 1.5.0_22 Sun Microsystems, Inc. Binary Code License Agreement http://java.sun.com/j2se/1.5.0 XDCtools core functionality is implemented in Java. Also required by the Rhino JavaScript engine shipped with XDCtools.
Although the following tools are not required, they are optionally shipped with XDCtools distributions to ensure consistent behavior across various development platforms.
Exe Version License From Description
zip, unzip 2.3 and 5.50 info-zip http://www.info-zip.org command line utilities to zip and unzip package releases
tar 1.13 GPL v2 http://www.gnu.org/software/tar command line utilities to archive package directories
sh cygwin 1.5.25-15 GPL v2 http://cygwin.com (Windows only) korn shell compatible shell used by GNU make
All other files that are part of XDCtools are licensed under either EPL v1.0 or dual-licensed under EDL v1.0.
generated on Tue, 01 Feb 2011 01:39:00 GMT