1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Log.xdc ========
15 */
16
17 /*!
18 * ======== Log ========
19 * Event logging manager
20 *
21 * RTSC modules and the application code generate `{@link #Event Log_Event}`
22 * events by calling the `Log` module's functions. The `Log` module then
23 * passes those events to an `{@link ILogger}` instance assigned to the event
24 * originating module, specified by that module's configuration parameter
25 * `common$.logger`. `ILogger` instances handle events, usually converting
26 * events to `{@link #EventRec Log_EventRec}` records prior to recording,
27 * transmitting, or displaying them.
28 *
29 * All events generated by a target module are stored and displayed by an
30 * `ILogger`, examples of which are instances of
31 * `{@link LoggerBuf xdc.runtime.LoggerBuf}` or
32 * `{@link LoggerSys xdc.runtime.LoggerSys}`. At runtime, modules
33 * generate events through this module, rather than invoking directly their
34 * `ILogger`s. By doing so, modules can be configured to use different
35 * `ILogger` implementations without any changes to their source code.
36 *
37 * A logger instance can accept `Log` events from any module, but a module
38 * can put `Log` events to only one logger instance. There can be one or
39 * more logger instances in a system. All `Log` calls that are not in a
40 * module are controlled by the module `{@link Main xdc.runtime.Main}`.
41 * For example, top-level application code or any existing sources that
42 * simply call the `Log` or `Assert` methods implicitly use the logger
43 * associated with the `Main` module.
44 *
45 * The generation of a `Log` event is controlled by a module's diagnostics
46 * mask, which is described in details in `{@link Diags}`. Each `Log` event
47 * is associated with a mask. `Log` events are generated only when a
48 * particular bit is set in both the `Log` event mask
49 * and the module's diagnostics mask. For example, a `Log` event mask with
50 * the `{@link Diags#USER1 USER1}` bit set is generated only when the `USER1`
51 * bit is also set in the module's diagnostics mask.
52 *
53 * There are two ways to generate `Log` events:
54 *
55 * @p(blist) 56 * - `{@link #write8 LOG_write()}`, which is tailored for module writers
57 * and takes full advantage of the XDC configuration model. For example,
58 * the message string associated with the `Log` event need not be a part of
59 * the final application, significantly reducing the "footprint overhead"
60 * of embedding diagnostics in deployed systems. The `Log_write[0-8]()`
61 * functions allow up to 8 values to be passed to the logger. They expect
62 * the logger to handle any formatting. A `Log` event type allows you to
63 * specify the type of event.
64 * - `{@link #print6 LOG_print()}`, which is designed for arbitrary C code.
65 * The `Log_print[0-6]()` functions allow up to 6 values to be passed along
66 * with a printf-like format string to the logger. They handle printf-style
67 * formatting.
68 * @p 69 *
70 * Both functions are controlled by the module's diagnostics mask. Their
71 * storage or output is defined by the logger that is assigned to the
72 * module that calls the `Log` methods or to the
73 * `{@link Main xdc.runtime.Main}` module if the caller is not part of a
74 * module.
75 *
76 * The `Log` function call sites are implemented in such a way that an
77 * optimizer can completely eliminate `Log` code from the program if the
78 * `Log` functions have been permanently disabled at configuration time. If
79 * the `Log` functions are permanently turned on at configuration time,
80 * then the optimizer can eliminate all runtime conditional checking and
81 * simply invoke the `Log` functions directly. Runtime checking is performed
82 * only when the `Log` functions are configured to be runtime modifiable.
83 *
84 * The Log calls can also be completely removed by defining the symbol
85 * `xdc_runtime_Log_DISABLE_ALL`. This can be done on the compile line, e.g.
86 * `-Dxdc_runtime_Log_DISABLE_ALL`. This will completely remove the `Log`
87 * statements from any code compiled with this flag, regardless of the
88 * application's logging configuration or your compiler's optimization
89 * settings.
90 *
91 * It is also possible to remove all logging except for
92 * `{@link #error Log_error}`, `{@link #warning Log_warning}`, or
93 * `{@link #info Log_info}` statements. This is done by first defining
94 * `xdc_runtime_Log_DISABLE_ALL`, followed by defining one or more of the
95 * symbols below to leave that type of logging enabled:
96 * @p(blist) 97 * - `xdc_runtime_Log_ENABLE_ERROR`
98 * - `xdc_runtime_Log_ENABLE_WARNING`
99 * - `xdc_runtime_Log_ENABLE_INFO`
100 * @p 101 * For example, to disable all `Log` statements except for `Log_error`, add
102 * the following to the compile line:
103 * @p(code) 104 * -Dxdc_runtime_Log_DISABLE_ALL -Dxdc_runtime_Log_ENABLE_ERROR
105 * @p 106 *
107 * @a(Examples) 108 * Example 1: The following example defines a `Log` event, uses that `Log`
109 * event in a module, and configures the program to generate the `Log`
110 * event. In this example, both `USER1` and `USER2` bits are set in the
111 * event mask. This means that if either bit is set in the module's
112 * diagnostics mask, then the `Log` event will be generated.
113 *
114 * This is a part of the XDC specification file for the `Mod` module
115 * (Mod.xdc):
116 *
117 * @p(code) 118 * import xdc.runtime.Diags;
119 * import xdc.runtime.Log;
120 *
121 * config Log.Event L_someEvent = {
122 * mask: Diags.USER1 | Diags.USER2,
123 * level: Diags.LEVEL1,
124 * msg: "my log event message, arg1: 0x%x, arg2: 0x%x"
125 * };
126 * @p 127 *
128 * This is a part of the C code implementation of the Mod module:
129 *
130 * @p(code) 131 * #include <xdc/runtime/Log.h>
132 * UInt x, y;
133 *
134 * Log_write2(Mod_L_someEvent, (IArg)x, (IArg)y);
135 * @p 136 *
137 * The following configuration script demonstrates how the application might
138 * control the `Log` statements embedded in the `Mod` module at configuration
139 * time. In this case, the configuration script arranges for the `Log`
140 * statements within the `Mod` module (shown above) to always generate events.
141 * Without these configuration statements, no `Log` events would be generated
142 * by this module.
143 *
144 * This is part of the XDC configuration file for the application:
145 *
146 * @p(code) 147 * var Diags = xdc.useModule('xdc.runtime.Diags');
148 * var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
149 * var Mod = xdc.useModule('my.pkg.Mod');
150 * Mod.common$.diags_USER1 = Diags.ALWAYS_ON;
151 * Mod.common$.logger = LoggerSys.create();
152 * @p 153 *
154 * @p(html) 155 * <hr />
156 * @p 157 *
158 * Example 2: The following XDC configuration statements turn on enter
159 * and exit logging at configuration time for a module. Without any other
160 * changes in the runtime code, every time a module `Mod`'s function is
161 * being called or exits, an event will be logged.
162 *
163 * @p(code) 164 * var Diags = xdc.useModule('xdc.runtime.Diags');
165 * var Mod = xdc.useModule('my.pkg.Mod');
166 *
167 * Mod.common$.diags_ENTER = Diags.ALWAYS_ON;
168 * Mod.common$.diags_EXIT = Diags.ALWAYS_ON;
169 * @p 170 *
171 * @p(html) 172 * <hr />
173 * @p 174 *
175 * Example 3: The following example configures a module to support enter and
176 * exit logging, but defers the actual activation and deactivation of the
177 * logging until runtime. See the `{@link Diags#setMask Diags_setMask()}`
178 * function for details on specifying the control string.
179 *
180 * This is a part of the XDC configuration file for the application:
181 *
182 * @p(code) 183 * var Diags = xdc.useModule('xdc.runtime.Diags');
184 * var Mod = xdc.useModule('my.pkg.Mod');
185 *
186 * Mod.common$.diags_ENTER = Diags.RUNTIME_OFF;
187 * Mod.common$.diags_EXIT = Diags.RUNTIME_OFF;
188 * @p 189 *
190 * This is a part of the C code for the application:
191 *
192 * @p(code) 193 * // turn on enter and exit logging in the module
194 * Diags_setMask("my.pkg.Mod+EX");
195 *
196 * // turn off enter and exit logging in the module
197 * Diags_setMask("my.pkg.Mod-EX");
198 * @p 199 */
200
201 @CustomHeader
202
203 module Log {
204
205 /*!
206 * ======== NUMARGS ========
207 * Maximum number of arguments supported in `Log` events.
208 */
209 const Int NUMARGS = 8;
210
211 /*!
212 * ======== PRINTFID ========
213 * The `EventId` for `Log_print()` events
214 */
215 const EventId PRINTFID = 0;
216
217 /*!
218 * ======== EventDesc ========
219 * `Log` event descriptor
220 *
221 * Each `Log` event is defined by a `Log` event descriptor.
222 *
223 * The `mask` defines which bits in the module's diagnostics mask
224 * enable this `Log` event. Events "posted" via `Log_write` are only
225 * written to the underlying logger if one of the mask's bits matches
226 * the caller's module diagnostics settings (see
227 * `{@link xdc.runtime.Types#common$}`).
228 *
229 * The 'level' defines the event level of the event. While the diags
230 * bits selected in the 'mask' signify the "category" of the event (e.g.
231 * Entry/Exit, Analysis, Info), the 'level' field allows you to assign
232 * a "priority" or "detail level" to the event relative to other events in
233 * that category. There are four event levels defined by
234 * '{@link xdc.runtime.Diags#EventLevel}'.
235 *
236 * Filtering of events by level is handled by the ILogger implementation.
237 * ILogger implementations which also implement the {@link IFilterLogger}
238 * interface support filtering of events based on priority level.
239 *
240 * Specifying an event level is optional. Events that don't specify a
241 * level will receive Diags.LEVEL1 by default, making them the highest
242 * priority and ensuring that they will not inadvertently be filtered out
243 * by level-based filtering.
244 *
245 * The `msg` defines a printf style format string that defines how to
246 * render the arguments passed along the event in a `Log_write` call.
247 * For a description of the allowable format strings see
248 * `{@link #print6}`.
249 *
250 * @see #write8
251 * @see #print6
252 */
253 metaonlystruct EventDesc {
254 Diags.Mask mask; /*! event enable mask */
255 Diags.EventLevel level; /*! event level relative to other events */
256 String msg; /*! event "printf" message format string */
257 };
258
259 /*!
260 * ======== EventRec ========
261 * The target representation of a recorded event
262 *
263 * This structure defines how events are recorded on the target.
264 */
265 struct EventRec {
266 Types.Timestamp64 tstamp; /*! time event was written */
267 Bits32 serial; /*! serial number of event */
268 Types.Event evt; /*! target encoding of an Event */
269 IArg arg[NUMARGS]; /*! arguments passed via Log_write/print */
270 }
271
272 /*!
273 * ======== Event ========
274 * `Log` event type
275 *
276 * An `Event` is represented on the target as a 32-bit value that can
277 * be decoded offline to recover the `Event` information defined in
278 * a corresponding metaonly `EventDesc`. In addition, `Event`s may be
279 * decoded at runtime via methods provided in this module; see
280 * `{@link #getMask}` and `{@link #getEventId}`.
281 *
282 * When an event is "raised" a `{@link Types#Event Types_Event}` is
283 * created which has the same event ID as the `Log_Event` but also
284 * encodes the module ID of the caller. This new event is passed to
285 * the underlying `{@link ILogger}` module along with any arguments
286 * associated with the event.
287 *
288 * @see #getMask
289 * @see #getEventId
290 */
291 @Encoded typedef EventDesc Event;
292
293 /*!
294 * ======== EventId ========
295 * Unique ID embedded in each `{@link #Event}`
296 *
297 * This ID must be used to compare two `Event`s for equality. Event
298 * ids are not guaranteed to remain constant between different
299 * configurations of an application. For example, adding a module
300 * may cause the event ids of another module to change.
301 *
302 * However, event ids declared by a module are guaranteed to be
303 * consecutive values starting from the first declared
304 * `{@link #Event Log_Event}` and increasing to the last declared
305 * event. As a result, clients of a module can efficiently test ranges
306 * of events and modules can add new events, such as internal trace
307 * events, without breaking clients; simply be careful to add new events
308 * after any existing events in you module's `.xdc` specification.
309 *
310 * @see #getEventId
311 * @see #Event
312 */
313 typedef Types.RopeId EventId;
314
315 /*!
316 * ======== L_construct ========
317 * Lifecycle event posted when an instance is constructed
318 */
319 config Log.Event L_construct = {
320 mask: Diags.LIFECYCLE,
321 msg: "<-- construct: %p('%s')"
322 };
323
324 /*!
325 * ======== L_create ========
326 * Lifecycle event posted when an instance is created
327 */
328 config Log.Event L_create = {
329 mask: Diags.LIFECYCLE,
330 msg: "<-- create: %p('%s')"
331 };
332
333 /*!
334 * ======== L_destruct ========
335 * Lifecycle event posted when an instance is destructed
336 */
337 config Log.Event L_destruct = {
338 mask: Diags.LIFECYCLE,
339 msg: "--> destruct: (%p)"
340 };
341
342 /*!
343 * ======== L_delete ========
344 * Lifecycle event posted when an instance is deleted
345 */
346 config Log.Event L_delete = {
347 mask: Diags.LIFECYCLE,
348 msg: "--> delete: (%p)"
349 };
350
351 /*!
352 * ======== L_error ========
353 * Error event posted by Log_errorX API
354 *
355 * This event is marked as a STATUS event and given the priority level
356 * of ERROR.
357 *
358 * This event prints the Log call site (%$F) and a format string (%$S)
359 * which is recursively formatted with any addition arguments.
360 */
361 config Log.Event L_error = {
362 mask: Diags.STATUS,
363 level: Diags.ERROR,
364 msg: "ERROR: %$F%$S"
365 };
366
367 /*!
368 * ======== L_warning ========
369 * Warning event posted by Log_warningX API
370 *
371 * This event is marked as a STATUS event and given the priority level of
372 * WARNING.
373 *
374 * This event prints the Log call site (%$F) and a format string (%$S)
375 * which is recursively formatted with any addition arguments.
376 */
377 config xdc.runtime.Log.Event L_warning = {
378 mask: Diags.STATUS,
379 level: Diags.WARNING,
380 msg: "WARNING: %$F%$S"
381 };
382
383 /*!
384 * ======== L_info ========
385 * Info event posted by Log_infoX API
386 *
387 * This event is marked as an INFO event. The event priority is not
388 * specified in the event definition. Rather, it is specified as an
389 * argument to the Log_infoX APIs.
390 *
391 * This event prints the Log call site (%$F) and a format string (%$S)
392 * which is recursively formatted with any addition arguments.
393 */
394 config xdc.runtime.Log.Event L_info = {
395 mask: Diags.INFO,
396 msg: "%$F%$S"
397 };
398
399 /*!
400 * ======== getMask ========
401 * Get the `Diags` mask for the specified (encoded) event
402 *
403 * @param(evt) the `Log` event encoding a mask and event ID
404 *
405 * @a(returns) `Diags` mask for the specified event
406 */
407 @Macro Diags.Mask getMask(Event evt);
408
409 /*!
410 * ======== getRope ========
411 * Get RopeId of the Event.msg for the specified (encoded) event
412 * @_nodoc 413 */
414 @Macro Text.RopeId getRope(Event evt);
415
416 /*!
417 * ======== getEventId ========
418 * Get event ID of the specified (encoded) event
419 *
420 * This method is used to compare "known" `Log` events with
421 * "raised" `{@link Types#Event Types_Event}`.
422 *
423 * @param(evt) the `Log` event encoding a mask and event ID
424 *
425 * @a(returns) event ID of the specified event
426 *
427 * @see Types#getEventId
428 */
429 @Macro EventId getEventId(Event evt);
430
431 /*!
432 * ======== print0 ========
433 * Generate a `Log` "print event" with 0 arguments
434 *
435 * @see #print6
436 */
437 @Macro Void print0(Diags.Mask mask, String fmt);
438
439 /*!
440 * ======== print1 ========
441 * Generate a `Log` "print event" with 1 argument
442 *
443 * @see #print6
444 */
445 @Macro Void print1(Diags.Mask mask, String fmt, IArg a1);
446
447 /*!
448 * ======== print2 ========
449 * Generate a `Log` "print event" with 2 arguments
450 *
451 * @see #print6
452 */
453 @Macro Void print2(Diags.Mask mask, String fmt, IArg a1, IArg a2);
454
455 /*!
456 * ======== print3 ========
457 * Generate a `Log` "print event" with 3 arguments
458 *
459 * @see #print6
460 */
461 @Macro Void print3(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3);
462
463 /*!
464 * ======== print4 ========
465 * Generate a `Log` "print event" with 4 arguments
466 *
467 * @see #print6
468 */
469 @Macro Void print4(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3,
470 IArg a4);
471
472 /*!
473 * ======== print5 ========
474 * Generate a `Log` "print event" with 5 arguments
475 *
476 * @see #print6
477 */
478 @Macro Void print5(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3,
479 IArg a4, IArg a5);
480
481 /*!
482 * ======== print6 ========
483 * Generate a `Log` "print event" with 6 arguments
484 *
485 * As a convenience to C (as well as assembly language) programmers,
486 * the `Log` module provides a variation of the ever-popular `printf`
487 * function.
488 * The `print[0-6]` functions generate a `Log` "print event" and route
489 * it to the current module's logger.
490 *
491 * The arguments passed to `print[0-6]` may be characters, integers,
492 * strings, or pointers. However, because the declared type of the
493 * arguments is `{@link xdc IArg}`, all pointer arguments must be cast
494 * to an `IArg` type. `IArg` is an integral type large enough to hold
495 * any pointer or an `int`. So, casting a pointer to an `IArg` does
496 * not cause any loss of information and C's normal integer conversions
497 * make the cast unnecessary for integral arguments.
498 *
499 * The format string can use the following conversion characters.
500 * However, it is important to recall that all arguments referenced by
501 * these conversion characters have been converted to an `IArg`
502 * prior to conversion; so, the use of "length modifiers" should be
503 * avoided.
504 *
505 * @p(code) 506 * Conversion Character Description
507 * ------------------------------------------------
508 * %c Character
509 * %d Signed integer
510 * %u Unsigned integer
511 * %x Unsigned hexadecimal integer
512 * %o Unsigned octal integer
513 * %s Character string
514 * %p Pointer
515 * %f Single precision floating point (float)
516 * @p 517 *
518 * Format strings, while very convenient, are a well known source of
519 * portability problems: each format specification must precisely match
520 * the types of the arguments passed. Underlying "printf" functions use
521 * the format string to determine how far to advance through their
522 * argument list. For targets where pointer types and integers are the
523 * same size there are no problems. However, suppose a target's pointer
524 * type is larger than its integer type. In this case, because integer
525 * arguments are widened to be of type `IArg`, a format specification of
526 * "%d" causes an underlying `printf()` implementation to read the
527 * extended part of the integer argument as part of the next argument(!).
528 *
529 * To get around this problem and still allow the use of "natural"
530 * format specifications (e.g., `%d` and `%x` with optional width
531 * specifications), `{@link System#aprintf()}` is used which assumes
532 * that all arguments have been widened to be of type `IArg`.
533 *
534 * See `{@link System#printf}` for complete details.
535 *
536 * The `%f` format specifier is used to print a single precision float
537 * value. Note that `%f` assumes that sizeof(Float) <= sizeof(IArg).
538 * Most clients that interpret float values except that they are
539 * represented in IEEE 754 floating point format. Therefore, it is
540 * recommended that the float values are converted into that format prior
541 * to supplying the values to `Log` functions in cases where targets do
542 * not generate the float values in IEEE 754 floating point format by
543 * default.
544 *
545 * The first argument to a Log_print call is the diags category to be
546 * associated with the event.
547 *
548 * It is also possible to associate an event level with the event to
549 * enable filtering of events based on event level. Conceptually, it is
550 * best to regard the event level as completely separate from the event's
551 * diags category; however, the priority value actually occupies a part
552 * of the diags mask. For this reason, it is possible to specify an event
553 * level by ORing the level with the diags mask. For example, to print
554 * an INFO event of LEVEL2, you'd simply write:
555 * (Diags.INFO | Diags.LEVEL2)
556 *
557 * Specifying an event level is optional. Log_print calls which do not
558 * specify a level will receive the highest priority by default.
559 *
560 * @param(mask) enable bits and optional detail level for this event
561 * @param(fmt) a `printf` style format string
562 * @param(a1) value for first format conversion character
563 * @param(a2) value for second format conversion character
564 * @param(a3) value for third format conversion character
565 * @param(a4) value for fourth format conversion character
566 * @param(a5) value for fifth format conversion character
567 * @param(a6) value for sixth format conversion character
568 *
569 * @a(Examples) 570 * The following example demonstrates a typical usage.
571 * @p(code) 572 * String list[];
573 * UInt i;
574 *
575 * Log_print2(Diags_USER2, "list[%u] = %s\n", i, (IArg)list[i]);
576 * @p 577 * Note that the `IArg` cast above is only necessary for pointer
578 * arguments; C's normal parameter conversions implicitly convert
579 * integral arguments.
580 */
581 @Macro Void print6(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3,
582 IArg a4, IArg a5, IArg a6);
583
584 /*!
585 * ======== error0 ========
586 * Generate a `Log` "error event" with 0 arguments
587 *
588 * @see #error5
589 */
590 @Macro Void error0(String fmt);
591
592 /*!
593 * ======== error1 ========
594 * Generate a `Log` "error event" with 1 argument
595 *
596 * @see #error5
597 */
598 @Macro Void error1(String fmt, IArg a1);
599
600 /*!
601 * ======== error2 ========
602 * Generate a `Log` "error event" with 2 arguments
603 *
604 * @see #error5
605 */
606 @Macro Void error2(String fmt, IArg a1, IArg a2);
607
608 /*!
609 * ======== error3 ========
610 * Generate a `Log` "error event" with 3 arguments
611 *
612 * @see #error5
613 */
614 @Macro Void error3(String fmt, IArg a1, IArg a2, IArg a3);
615
616 /*!
617 * ======== error4 ========
618 * Generate a `Log` "error event" with 4 arguments
619 *
620 * @see #error5
621 */
622 @Macro Void error4(String fmt, IArg a1, IArg a2, IArg a3,
623 IArg a4);
624
625 /*!
626 * ======== error5 ========
627 * Generate a `Log` "error event" with 5 arguments
628 *
629 * The Log_error APIs are intended to allow users to easily log error
630 * events in their code. Similar to the Log_print APIs, Log_error does not
631 * require that you define an event. You simply pass an informative error
632 * string which can optionally be formatted with additional arguments. The
633 * error is logged with the predefined event {@link #L_error}.
634 *
635 * Log_error prepends a string to the message which identifies it as an
636 * ERROR and specifies the filename and line number of the Log_error call
637 * site. A simple example:
638 *
639 * @p(code) 640 * Log_error0("Invalid argument");
641 * @p 642 * This event will be formatted as (assuming that the above call was line
643 * 35 of "MyCode.c")
644 * @p(code) 645 * ERROR at "MyCode.c", line 35: Invalid argument
646 * @p 647 *
648 * Users may provide additional information in the error event, such as
649 * a predefined error code or details of the error. These additional
650 * values will be used to format the string passed to Log_error.
651 * @see #print6 for information about format strings.
652 *
653 * Log_error does not use a variable length argument list--you must call
654 * the appropriate Log_errorX API based on the number of arguments.
655 *
656 * @param(fmt) a reference to a constant error string / fmt string
657 * @param(a1) value for an additional parameter (e.g. an error code)
658 * @param(a2) value for an additional parameter
659 * @param(a3) value for an additional parameter
660 * @param(a4) value for an additional parameter
661 * @param(a5) value for an additional parameter
662 *
663 * @a(Examples) 664 * The following example demonstrates a typical usage.
665 * @p(code) 666 * Int myArg;
667 *
668 * Log_error1("Invalid argument: %d", myArg);
669 * @p 670 * The above event is formatted as, for example:
671 * @p(code) 672 * ERROR: "MyCode.c", line 35: Invalid argument: -1
673 * @p 674 */
675 @Macro Void error5(String fmt, IArg a1, IArg a2, IArg a3,
676 IArg a4, IArg a5);
677
678 /*!
679 * ======== warning0 ========
680 * Generate a `Log` "warning event" with 0 arguments
681 *
682 * @see #warning5
683 */
684 @Macro Void warning0(String fmt);
685
686 /*!
687 * ======== warning1 ========
688 * Generate a `Log` "warning event" with 1 argument
689 *
690 * @see #warning5
691 */
692 @Macro Void warning1(String fmt, IArg a1);
693
694 /*!
695 * ======== warning2 ========
696 * Generate a `Log` "warning event" with 2 arguments
697 *
698 * @see #warning5
699 */
700 @Macro Void warning2(String fmt, IArg a1, IArg a2);
701
702 /*!
703 * ======== warning3 ========
704 * Generate a `Log` "warning event" with 3 arguments
705 *
706 * @see #warning5
707 */
708 @Macro Void warning3(String fmt, IArg a1, IArg a2, IArg a3);
709
710 /*!
711 * ======== warning4 ========
712 * Generate a `Log` "warning event" with 4 arguments
713 *
714 * @see #warning5
715 */
716 @Macro Void warning4(String fmt, IArg a1, IArg a2, IArg a3,
717 IArg a4);
718
719 /*!
720 * ======== warning5 ========
721 * Generate a `Log` "warning event" with 5 arguments
722 *
723 * The Log_warning APIs provide the same features as the Log_error APIs,
724 * but are used to specifically log "warning" events.
725 * @see #error5
726 *
727 * The Log_warning APIs are equivalent to the Log_error APIs except that
728 * they use the predefined {@link #L_warning} event. Log_warning prepends
729 * a string to the message which identifies it as a WARNING and specifies
730 * the filename and line number of the Log_warning call site.
731 *
732 * @param(fmt) reference to a constant warning string / fmt string
733 * @param(a1) value for an additional parameter (e.g. a warning code)
734 * @param(a2) value for an additional parameter
735 * @param(a3) value for an additional parameter
736 * @param(a4) value for an additional parameter
737 * @param(a5) value for an additional parameter
738 *
739 * @a(Examples) 740 * The following example demonstrates a typical usage.
741 * @p(code) 742 * Int myArg;
743 *
744 * Log_warning1("Value may be too high: %d", myArg);
745 * @p 746 * The above event is formatted as:
747 * @p(code) 748 * WARNING: "MyCode.c", line 50: Value may be too high: 4096
749 * @p 750 */
751 @Macro Void warning5(String fmt, IArg a1, IArg a2, IArg a3,
752 IArg a4, IArg a5);
753
754 /*!
755 * ======== info0 ========
756 * Generate a `Log` "info event" with 0 arguments
757 *
758 * @see #info5
759 */
760 @Macro Void info0(String fmt);
761
762 /*!
763 * ======== info1 ========
764 * Generate a `Log` "info event" with 1 argument
765 *
766 * @see #info5
767 */
768 @Macro Void info1(String fmt, IArg a1);
769
770 /*!
771 * ======== info2 ========
772 * Generate a `Log` "info event" with 2 arguments
773 *
774 * @see #info5
775 */
776 @Macro Void info2(String fmt, IArg a1, IArg a2);
777
778 /*!
779 * ======== info3 ========
780 * Generate a `Log` "info event" with 3 arguments
781 *
782 * @see #info5
783 */
784 @Macro Void info3(String fmt, IArg a1, IArg a2, IArg a3);
785
786 /*!
787 * ======== info4 ========
788 * Generate a `Log` "info event" with 4 arguments
789 *
790 * @see #info5
791 */
792 @Macro Void info4(String fmt, IArg a1, IArg a2, IArg a3, IArg a4);
793
794 /*!
795 * ======== info5 ========
796 * Generate a `Log` "info event" with 5 arguments
797 *
798 * The Log_info APIs are provided for easily logging generic
799 * "informational" events with call site information. They are similar to
800 * the Log_print APIs in that they do not require you to define an event--
801 * you simply pass an informative printf-style string which can optionally
802 * be formatted with additional arguments. The info record is logged with
803 * the predefined event '{@link #L_info}'.
804 *
805 * The Log_info APIs log the {@link #L_info} event which uses the 'INFO'
806 * diags category. They do not allow you to specify an event priority.
807 *
808 * Log_info prepends the filename and line number of the call site to the
809 * message.
810 *
811 * @param(fmt) reference to a constant event string / fmt string
812 * @param(a1) value for an additional parameter (e.g. an event code)
813 * @param(a2) value for an additional parameter
814 * @param(a3) value for an additional parameter
815 * @param(a4) value for an additional parameter
816 * @param(a5) value for an additional parameter
817 *
818 * @a(Examples) 819 * The following example demonstrates a typical usage.
820 * @p(code) 821 * Int load;
822 *
823 * Log_info1("Current load: %d", load);
824 * @p 825 * The above event is formatted as, for example:
826 * @p(code) 827 * "MyCode.c", line 15: Current load: 25
828 * @p 829 */
830 @Macro Void info5(String fmt, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5);
831
832 /*!
833 * ======== put0 ========
834 * Unconditionally put the specified Log event with 0 arguments
835 *
836 * @see #put4
837 */
838 @Macro Void put0(Log.Event evt, Types.ModuleId mid);
839
840 /*!
841 * ======== put1 ========
842 * Unconditionally put the specified Log event and 1 argument
843 *
844 * @see #put4
845 */
846 @Macro Void put1(Log.Event evt, Types.ModuleId mid, IArg a1);
847
848 /*!
849 * ======== put2 ========
850 * Unconditionally put the specified Log event and 2 arguments
851 *
852 * @see #put4
853 */
854 @Macro Void put2(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2);
855
856 /*!
857 * ======== put4 ========
858 * Unconditionally put the specified Log event
859 *
860 * This method unconditionally puts the specified `{@link Event}`
861 * `evt` into the log. The `{@link Types#ModuleId}` `mid` should be the
862 * module ID of the module which is putting the event.
863 *
864 * @param(evt) the Log event to put into the log
865 * @param(mid) module ID of the module putting the event
866 * @param(a1) value for first format conversion character
867 * @param(a2) value for second format conversion character
868 * @param(a3) value for third format conversion character
869 * @param(a4) value for fourth format conversion character
870 *
871 * @see #put8
872 */
873 @Macro Void put4(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
874 IArg a3, IArg a4);
875
876 /*!
877 * ======== put8 ========
878 * Unconditionally put the specified Log event and 8 arguments
879 *
880 * @see #put4
881 */
882 @Macro Void put8(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
883 IArg a3, IArg a4, IArg a5, IArg a6, IArg a7, IArg a8);
884
885 /*!
886 * ======== write0 ========
887 * Generate a `Log` event with 0 arguments
888 *
889 * @see #write8
890 */
891 @Macro Void write0(Event evt);
892
893 /*!
894 * ======== write1 ========
895 * Generate a `Log` event with 1 argument
896 *
897 * @see #write8
898 */
899 @Macro Void write1(Event evt, IArg a1);
900
901 /*!
902 * ======== write2 ========
903 * Generate a `Log` event with 2 arguments
904 *
905 * @see #write8
906 */
907 @Macro Void write2(Event evt, IArg a1, IArg a2);
908
909 /*!
910 * ======== write3 ========
911 * Generate a `Log` event with 3 arguments
912 *
913 * @see #write8
914 */
915 @Macro Void write3(Event evt, IArg a1, IArg a2, IArg a3);
916
917 /*!
918 * ======== write4 ========
919 * Generate a `Log` event with 4 arguments
920 *
921 * @see #write8
922 */
923 @Macro Void write4(Event evt, IArg a1, IArg a2, IArg a3, IArg a4);
924
925 /*!
926 * ======== write5 ========
927 * Generate a `Log` event with 5 arguments
928 *
929 * @see #write8
930 */
931 @Macro Void write5(Event evt, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5);
932
933 /*!
934 * ======== write6 ========
935 * Generate a `Log` event with 6 arguments
936 *
937 * @see #write8
938 */
939 @Macro Void write6(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
940 IArg a5, IArg a6);
941
942 /*!
943 * ======== write7 ========
944 * Generate a `Log` event with 7 arguments
945 *
946 * @see #write8
947 */
948 @Macro Void write7(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
949 IArg a5, IArg a6, IArg a7);
950
951 /*!
952 * ======== write8 ========
953 * Generate a `Log` event with 8 arguments
954 *
955 * If the mask in the specified `Log` event has any bit set which is
956 * also set in the current module's diagnostics mask, then this call to
957 * write will "raise" the given `Log` event.
958 *
959 * @param(evt) the `Log` event to write
960 * @param(a1) value for first format conversion character
961 * @param(a2) value for second format conversion character
962 * @param(a3) value for third format conversion character
963 * @param(a4) value for fourth format conversion character
964 * @param(a5) value for fifth format conversion character
965 * @param(a6) value for sixth format conversion character
966 * @param(a7) value for seventh format conversion character
967 * @param(a8) value for eighth format conversion character
968 */
969 @Macro Void write8(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
970 IArg a5, IArg a6, IArg a7, IArg a8);
971
972 /*!
973 * ======== doPrint ========
974 * Render an event as text via `{@link System#printf System_printf}`
975 *
976 * This method is not gated and may make more than one call to
977 * `System_printf`. This utility method is typically used within the
978 * implementation of a logger which initializes
979 * `{@link #EventRec Log_EventRec}` structures based on `Log` events
980 * produced by the application.
981 *
982 * @param(evRec) a non`NULL` pointer to an initialized `Log_EventRec`
983 * structure to be formated via
984 * `{@link System#printf System_printf}`.
985 */
986 Void doPrint(EventRec *evRec);
987
988 /*!
989 * @_nodoc 990 * ======== lookupEventMessage ========
991 * Returns the format string for the event with the given id.
992 */
993 function lookupEventMessage(eventId);
994
995 /*!
996 * @_nodoc 997 * ======== getTargetArgSize ========
998 * Returns the target size of a record argument in bytes (not MAUs).
999 */
1000 function getTargetArgSize();
1001
1002 /*!
1003 * @_nodoc 1004 * ======== lookupEventName ========
1005 */
1006 function lookupEventName(eventId);
1007
1008 /*!
1009 * @_nodoc 1010 * ======== lookupModuleName ========
1011 */
1012 function lookupModuleName(modId);
1013
1014 /*!
1015 * @_nodoc 1016 * ======== getTargetEventRecSize ========
1017 * Returns the record size in bytes (not MAUs).
1018 */
1019 function getTargetEventRecSize();
1020
1021 internal:
1022
1023 /*
1024 * ======== idToInfo ========
1025 * Map event ID strings into a string of the form <eventName>::<eventMsg>
1026 */
1027 metaonlyconfig String idToInfo[string] = [];
1028
1029 }
1030 /*
1031 * @(#) xdc.runtime; 2, 1, 0,299; 1-26-2011 10:39:22; /db/ztree/library/trees/xdc/xdc-v56x/src/packages/
1032 */
1033