package xdc.bld |
![](../../Arrow_right.png) |
The XDC Build Model
This package contains the XDC Build Model and the interfaces necessary
to extend the Build Model to handle new compiler tool chains. The
modules in this package (and the instances managed by these modules)
form the Build Object Model (BOM).
[
more ... ]
package xdc.bld [1, 0, 2] {
// The interface between code generation tool-chains and the XDC Build
Engine
// User-supplied filter of a target's command set
// Global build environment
// Model of a file that can be loaded and executed on a platform
// Model of a searchable collection of object files
// The manifest object for the release file post-processing model
// Model of a compiled (or assembled) form of a source file
// Package container populated by a build script
// Model of an archive of all files that are part of a release
// Model of a package repository
// Model of a script
// Model of a test
// Utility functions to simplify creation of targets and platforms
}
DETAILS
This package contains the XDC Build Model and the interfaces necessary
to extend the Build Model to handle new compiler tool chains. The
modules in this package (and the instances managed by these modules)
form the Build Object Model (BOM).
This model enables build scripts to declare the contents of each release
of a package. Based on these manifests, the Build Engine generates
makefiles that build the specified object files, libraries, and
executables, and archive these files into specified release files. In
addition, the generated makefiles are also capable of running collections
of executables with command line arguments (provided that the platforms
support this); e.g., regression tests.
NOTE
User supplied file names of source files, generated libraries and
executables must be limited to portable POSIX file names. That
means that only alphanumeric charaters, and '_', '.', and '-'
are allowed.
THROWS
XDCException exceptions are thrown for fatal errors. The following error
codes are reported in the exception message:
- xdc.bld.TARGET_CONFIG_ERROR
-
This error is reported whenever there is an error in
the target configuration file. Check the configuration script
for errors.
- xdc.bld.ROOTDIR_NOT_SET
-
This error is reported when the rootDir property for a target
has not been set in the target configuration script. Ensure
that this property is set correctly in the configuration
script.
- xdc.bld.PLATFORM_NOT_SET
-
This error is reported when either 1) the platform property for
a target has not been set in the target specification or the
target configuration script (config.bld) or 2) the build script
(package.bld) is setting the platform for a program to an
invalid value.
- xdc.bld.DUPLICATE_TARGET_ERROR
-
This error is reported when a same target is listed twice in
Bld.targets. Check xdc.bld.BuildEnvironment.targets
to find out how Bld.targets is constructed.
generated on Tue, 01 Feb 2011 01:39:13 GMT