From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
XDCscript - Instance-Object.$super
Instance of the inherited-interface
Contents |
Synopsis
| «inst».$super |
where «inst» is an instance object.
Description
The $super property of an instance object is a Instance object of the Instance type designated in the inherited-interface for the module managing this instance, or null if not specified.
See also
XDCscript - Instance-Object | Object containing per-instance-features of a module |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved