From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
XDCscript - Instance-Object.$module
The Module object that manages this instance
Contents |
Synopsis
| «inst».$module |
Description
The $module property of an instance object is the Module object that manages this instance.
See also
XDCscript - Instance-Object.$package | The Package object containing the module managing this instance |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved