From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
C - Module hasMask
Check for a module diagnostics mask
Contents |
Synopsis
| #include <«pkg»/«Mod».h> Bool «Mod»_Module_hasMask(void) /* does «Mod» have a diagnostic mask? */ |
Description
Every module «Mod» provides a parameterless macro named «Mod»_Module_hasMask() that returns a non-zero value in the event that the module has a diagnostics mask.
Since
This method was introduced in XDCtools release 3.15.
See also
C - Module_getMask | Get a module's diagnostics mask |
C - Module_setMask | Set a module's diagnostics mask |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved