| package xdc.tools.cdoc |
 |
RTSC documentation generator
cdoc is a package documentation generation utility. It builds a
directory of browsable HTML documentation using the meta-
information stored in RTSC packages.
[
more ... ]
package xdc.tools.cdoc [1, 0, 0, 0] {
// XDOC markup language examples for modules and interfaces
// Command implementation
// XDCspec doc markup language examples
}
USAGE
xs xdc.tools.cdoc [--help]
[-od:dir] [-title text] [--start package] [--indexonly] [--doxytags file] [--doxybase dir] [-h] [-n] [-b] [-s] [-P pkg-dir...|-Pr repo-dir...|-A]
OPTIONS
- -od
- Place the generated files in the named directory
- -title
- Generated HTML pages will show the string in the page title
- --start
- Set start page to specified package
The opening page is, by default, the documentation for the
alphabetically first package processed. This option allows
you to explicitly specify the package used.
If "" is specified, the start page will be blank.
If the package specified is not processed, no warning or error
results; it is assumed that when the documentation is used the
specified package documentation will exist.
- -s
- Include .xdc file sources
In the generated documentation for each .xdc file, link
to a pretty-printed view of the .xdc file source text.
- -P
- The subsequent directories are package directories
Generates documentation for each of the specified packages.
- -Pr
- The subsequent directories are repositories of packages
Generates documentation for all packages rooted in each of
the specified repositories.
- -A
- Generate documentation for all packages on the package path
- -b
- Generate a single "big" output
- -h
- Generate html pages only, not table of contents or index
- -n
- Generate nodoc'd docs
- --quiet
- Quiet mode
- --indexonly
- Generate index and table of contents only
- --doxytags
- Process doxygen links, using this argument
as the tag file
- --doxybase
- The directory containing doxygen html files
- --style
- Use specified style sheet
- -l
- Language to document. Deprecated
- -L
- Don't include dependent packages. Deprecated
DETAILS
cdoc is a package documentation generation utility. It builds a
directory of browsable HTML documentation using the meta-
information stored in RTSC packages.
This utility is invoked via the XDCtools xs command. In the
examples below we assume that the alias cdoc is defined as
follows:
$(XDCROOT)/xs xdc.tools.cdoc
where $(XDCROOT) is the installation directory of the XDCtools toolset.
EXAMPLES
In the examples below we assume that the alias cdoc is defined as
$(XDCROOT)/xs xdc.tools.cdoc, where $(XDCROOT) is the installation
directory of the XDCtools toolset.
1. To generate documentation for the package in the current working
directory:
Since no package is specified and no output directory is specified,
documentation is generated for the package in the current working
directory and the output is placed in the package's ./package/cdoc
sub-directory.
2. To generate documentation with the title "My Packages" for all
packages installed in the myPackages repository:
cdoc -title "My Packages" -Pr myPackages
Since no output directory was specified and documentation will be for
more than one package, the generated files are placed in the directory
./cdoc.
3. To generate documentation for the package located in ./ti/bios and
put results in the directory ./html.
NOTE
cdoc processes the XML files that are generated *after* a package
is built (actually after the .interfaces goal is built). One must first
build a package before generating its documentation. If you change a
.xdc file and re-run cdoc without rebuilding the package, the change
in the .xdc file will not show up in the generated docs.
When interatively updating a package's .xdc files and examining the
generated documentation, it is useful to define a command alias that
first "compiles" the package's .xdc files and then runs the cdoc tool.
For example, if your shell is Korn shell compatible, the following
command alias ensures that any changes in .xdc files will show up in the
generated documents:
function cdoc {
$XDCROOT/xdc .interfaces
$XDCROOT/xs xdc.tools.cdoc $*
}
generated on Tue, 18 Jan 2011 00:02:19 GMT