From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCspec - @Annex
This parameter or method has been added
| @Annex(N) |
This attribute can be applied to configuration parameters and functions. When new functions and configuration parameters need to be added to a module, adding @Annex(N) in front of them ensures that only R digit of the compatibility key needs to be changed. N must be an integer bigger than any of the integers used for @Annex in previous versions of the module.
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved