1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Cache.xdc ========
    15     */
    16    
    17    import xdc.runtime.Error;
    18    import xdc.runtime.knl.ICacheSupport;
    19    
    20    /*!
    21     *  ======== Cache ========
    22     *  Cache Services
    23     *
    24     *  The Cache module provide APIs to allow applications to maintain cache 
    25     *  coherency.
    26     *
    27     *  This module will use an OS specific delegate (back-end) to manipulate the 
    28     *  cache.
    29     *  This module has a module wide config parameter {@link #Proxy} which needs to
    30     *  be bound to an OS specific delegate before this module can be used.
    31     *  
    32     *  Here is an example showing how the proxy is bound to an BIOS 6.x specific 
    33     *  delegate.
    34     *   
    35     *  @p(code)
    36     *  var Cache = xdc.useModule('xdc.runtime.knl.Cache');
    37     *  Cache.Proxy = xdc.useModule('ti.sysbios.xdcruntime.CacheSupport');
    38     *  @p
    39     *
    40     *  Typically the package containing the delegates have a Settings module that 
    41     *  will bind all {@link xdc.runtime.knl} proxies. The following
    42     *  example sets up all the xdc.runtime.knl proxies.
    43     *   
    44     *  @p(code)
    45     *  xdc.useModule("ti.sysbios.xdcruntime.Settings");
    46     *  @p
    47     */
    48    
    49    module Cache
    50    {
    51        /*!
    52         *  ======== Proxy ========
    53         *  ICacheSupport proxy
    54         *
    55         *  Cache will use this proxy to access the cache hardware using
    56         *  OS specific APIs.
    57         */
    58        proxy Proxy inherits ICacheSupport;
    59        
    60        /*!
    61         *  ======== inv ========
    62         *  Invalidate range of memory for all cache(s)
    63         *
    64         *  Invalidate the range of memory within the specified starting
    65         *  address and byte count.  The range of addresses operated on
    66         *  gets quantized to whole cache lines in each cache.  All lines
    67         *  in range are invalidated for all cache types.
    68         *
    69         *  @param(blockPtr) start address of range to be invalidated
    70         *  @param(byteCnt)  number of bytes to be invalidated
    71         *  @param(wait)     wait until the operation is completed
    72         *  @param(eb)       error block
    73         *  @a(returns)      true for success; false for error.
    74         */
    75        Bool inv(Ptr blockPtr, SizeT byteCnt, Bool wait, Error.Block *eb);
    76    
    77        /*!
    78         *  ======== wb ========
    79         *  Writes back a range of memory from all cache(s)
    80         *
    81         *  Writes back the range of memory within the specified starting
    82         *  address and byte count.  The range of addresses operated on
    83         *  gets quantized to whole cache lines in each cache.  All lines
    84         *  within the range are left valid in all caches and the data
    85         *  within the range will be written back to the source memory.
    86         *
    87         *  @param(blockPtr) start address of range to be invalidated
    88         *  @param(byteCnt)  number of bytes to be invalidated
    89         *  @param(wait)     wait until the operation is completed
    90         *  @param(eb)       error block
    91         *  @a(returns)      true for success; false for error.
    92         */
    93        Bool wb(Ptr blockPtr, SizeT byteCnt, Bool wait, Error.Block *eb);
    94    
    95        /*!
    96         *  ======== wbInv ========
    97         *  Write back and invalidate range of memory.
    98         *
    99         *  Writes back and invalidates the range of memory within the
   100         *  specified starting address and byte count.  The range of
   101         *  addresses operated on gets quantized to whole cache lines in
   102         *  each cache.  All lines within the range are written back to the
   103         *  source memory and then invalidated for all cache types.
   104         *
   105         *  @param(blockPtr) start address of range to be invalidated
   106         *  @param(byteCnt)  number of bytes to be invalidated
   107         *  @param(wait)     wait until the operation is completed
   108         *  @param(eb)       error block
   109         *  @a(returns)      true for success; false for error.
   110         */
   111        Bool wbInv(Ptr blockPtr, SizeT byteCnt, Bool wait, Error.Block *eb);
   112    
   113        /*!
   114         *  ======== wait ========
   115         *  Wait for a previous cache operation to complete
   116         *
   117         *  Wait for the cache wb/wbInv/inv operation to complete.  A cache
   118         *  operation is not truly complete until it has worked its way
   119         *  through all buffering and all memory writes have landed in the
   120         *  source memory.
   121         *
   122         *  @param(eb)       error block
   123         *  @a(returns)      true for success; false for error.
   124         */
   125        Bool wait(Error.Block *eb);
   126    }
   127    /*
   128     *  @(#) xdc.runtime.knl; 1, 0, 0,105; 11-16-2010 11:20:23; /db/ztree/library/trees/xdc/xdc-v53x/src/packages/
   129     */
   130