1    /*!
     2     *  ======== Reset ========
     3     *  Startup reset function manager
     4     *
     5     *  This module defines the initial reset function and can be used without
     6     *  requiring any other `xdc.runtime` module.  The reset function is called
     7     *  as early as possible in the application startup and is intended for
     8     *  platform-specific hardware initialization.
     9     *
    10     *  @a(Warning)
    11     *  The reset function is _not_ supported on all platforms and, as a result,
    12     *  you should never place any "portable" code that is required for your
    13     *  application in this function.  Use the `@{link Startup}` module to
    14     *  define required application startup functions.
    15     *  
    16     *  @see Startup
    17     */
    18    @Template("xdc/runtime/Reset.xdt")
    19    metaonly module Reset
    20    {
    21        /*!
    22         *  ======== fxns ========
    23         *  List of functions to call at reset
    24         *
    25         *  This array defines the functions that will be executed by the reset
    26         *  initialization function (`xdc_runtime_Startup_reset__I`) _in addition
    27         *  to_ the function specified by `@{link Startup#resetFxn}`.
    28         *
    29         *  The following code fragment shows how to add the externally defined
    30         *  function `myReset()` to this array.
    31         *  @p(code)
    32         *      var Reset = xdc.useModule("xdc.runtime.Reset");
    33         *      Reset.fxns[Reset.fxns.length++] = "&myReset";
    34         *  @p
    35         *
    36         *  @a(Warning)
    37         *  Although the functions specified in `fxns[]` are ordinary C functions,
    38         *  they are often called _before_ the C runtime is fully initialized;
    39         *  e.g., they may be called _before_ static variables are initialized.
    40         *  Reset functions should only assume that a minimal execution stack has
    41         *  initialized.
    42         *
    43         *  @see Startup.resetFxn
    44         */
    45        metaonly config xdc.runtime.Startup.InitFxn fxns[] = [];
    46    }
    47    /*
    48     *  @(#) xdc.runtime; 2, 1, 0,296; 11-16-2010 11:20:24; /db/ztree/library/trees/xdc/xdc-v53x/src/packages/
    49     */
    50