1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*!
    14     *  ======== IFilterLogger ========
    15     *  Interface for supporting filtering of log events by detail level.
    16     *
    17     *  Filtering of events based on detail level is not inherently supported
    18     *  by the Log APIs as is filtering of events based on the diagnostics mask.
    19     *  
    20     *  Support for this type of filtering must be done by an ILogger 
    21     *  implementation. Not all users are interested in this filtering support,
    22     *  however, so it is not required that all ILogger implementations support it.
    23     *
    24     *  ILoggers which do intend to support filtering by detail level should 
    25     *  implement this interface, which extends the ILogger interface.
    26     *
    27     *  The {@link #setFilterLevel} and {@link #getFilterLevel} APIs support
    28     *  specification of a different filtering level for each of the diagnostics
    29     *  categories.
    30     */
    31    interface IFilterLogger inherits ILogger {
    32    
    33        /*!
    34         *  ======== filterByLevel ========
    35         *  Support filtering of events by event level.
    36         *
    37         *  To improve logging performance, this feature can be disabled by setting
    38         *  filterByLevel to false.
    39         */
    40        config Bool filterByLevel = false;
    41    
    42    instance:
    43    
    44        /*!
    45         *  ======== setFilterLevel ========
    46         *  Sets the level of detail that instances will log.
    47         *
    48         *  Events with the specified level or higher will be logged, events
    49         *  below the specified level will be dropped.
    50         *
    51         *  Events are filtered first by diags category, then by level. If an 
    52         *  event's diags category is disabled in the module's diags mask, then it 
    53         *  will be filtered out regardless of level. The event will not even be
    54         *  passed to the logger.
    55         *
    56         *  This API allows for setting the filtering level for more than one
    57         *  diags category at a time. The mask parameter can be a single category 
    58         *  or multiple categories combined, and the level will be set for all of
    59         *  those categories.   
    60         *
    61         *  @param(mask) The diags categories to set the level for
    62         *  @param(filterLevel) The new filtering level for the specified 
    63         *                      categories
    64         */
    65        Void setFilterLevel(Diags.Mask mask, Diags.EventLevel filterLevel);
    66        
    67        /*!
    68         *  ======== getFilterLevel ========
    69         *  Returns the mask of diags categories currently set to the specified 
    70         *  level.
    71         *
    72         *  See '{@link #setFilterLevel}' for an explanation of level filtering.
    73         */
    74        Diags.Mask getFilterLevel(Diags.EventLevel level);
    75    
    76    }
    77    /*
    78     *  @(#) xdc.runtime; 2, 1, 0,296; 11-16-2010 11:20:23; /db/ztree/library/trees/xdc/xdc-v53x/src/packages/
    79     */
    80