From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - Module-Object.$logWarning
Log a warning from this module
Contents |
Synopsis
| | «Mod».$logWarning(«msg», «obj»[, «prop»]) |
where «Mod» is the module from which the warning is sourced.
Parameters
- «msg»
- the string explaining the warning
- «obj»
- the typed object that is associated with the warning
- «prop»
- (optionally specified) property of «obj» that is associated with the warning
Description
A special method that "logs" a warning from the module «mod» with message «msg» associated with the typed object «obj». The optional argument, «prop», must be a property of «obj» and allows the module to specifically identify a configuration parameter associated with the warning.
Control returns to the caller of $logWarning so that multiple warnings can be logged. Warnings logged during the configuration validation phase (or earlier) do not prevent the generation phase from starting. Warnings logged at any time during configuration have no effect on the exit status.
Warning messages resulting from $logWarning have the following format:
| | warning: «Mod»: "«file»", line «num»: «obj» «prop»: «msg» |
where «file» and «line» are the file and line number where the call to $logWarning occurred.
Example
| Mod.xs | |
| | if (!("ti.mcu.msp430.csl.watchdog" in xdc.om)) { this.$logWarning("Watchdog timer has not been initialized.", this); } |
In the event that the warning above is triggered, a warning message similar to the following will be emitted.
| | warning: Mod: "Mod.xs", line 8: Mod: Watchdog timer has not been initialized. |
See also
| XDCscript - Module-Body.module$validate | Validate current domain object model |
| XDCscript - Module-Object.$logFatal | Throw fatal exception from this module |
| XDCscript - Module-Object.$logError | Log an error from this module |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |