1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    package xdc.bld;
    13    
    14    /*!
    15     *  ======== Manifest ========
    16     *  The manifest object for the release file post-processing model
    17     *
    18     *  Each package release corresponds to an archive of a subset of the
    19     *  developent package's contents.  The contents of each release are
    20     *  specified by an instance of the `{@link Release}` module.  Each instance
    21     *  of the `Release` module can optionally specify a "release script" that
    22     *  can modify each file prior to it being added to the archive.  This script
    23     *  runs in the context of the "release file post-processing" model.
    24     *
    25     *  This module is the root of the "release file post-processing" model.
    26     *  Each file in a release may be optionally post-processed by a filter
    27     *  specified in `{@link #filterMap}.`  Other fields of this module provide
    28     *  a release-specific "context" for the operation of the filters.  For
    29     *  example, a filter may use `{@link #packageName}`, `{@link #releaseName}`,
    30     *  and `{@link #buildCount}` to prefix all C sources with comments that
    31     *  identify where they originated.
    32     *
    33     *  All the fields of this module (except `{@link #filterMap}`) are initialized
    34     *  before a "release script" is run.  After the release script completes,
    35     *  the release archive is created according to the filters specifed in
    36     *  `{@link #filterMap}`.  Files that have no filter are copied without
    37     *  modification into the release.
    38     */
    39    metaonly module Manifest {
    40    
    41        /*!
    42         *  ======== Filter ========
    43         *  A file filter descriptor
    44         *
    45         *  @field(operation)  a JavaScript function that filters the specified
    46         *      input file and puts the results in specified output file; it is
    47         *      the output file that is archived as part of the release (not the
    48         *      input file).
    49         *
    50         *      The operation is called as follows:
    51         *      @p(code)
    52         *          operation(filter, src, dst, base)
    53         *      @p
    54         *      where:
    55         *      @p(dlist)
    56         *        -`filter`
    57         *              the filter object associated with the file being
    58         *              processed (which specified `operation` as the function
    59         *              to call)
    60         *        -`src`
    61         *              input file name (relative to the current working
    62         *              directory)
    63         *        -`dst`
    64         *              output file name (relative to the current working
    65         *              directory)
    66         *        -`base`
    67         *              string name of the file as it appears in the array
    68         *              `Manifest.files`; unlike `dst`, it does not contain a
    69         *              temporary directory name prefix.
    70         *
    71         *  @field(args)  array of arbitrary arguments passed to `operation`
    72         *      (as a field of the filter object passed as the first argument to
    73         *      `operation`)
    74         *
    75         *  @field(newFileName) the new name of the output file relative to the
    76         *      top of the archive.  Normally this name should include the
    77         *      package's name but, in situations where a release must support a
    78         *      non-RTSC conformant physical design, `newFileName` can be anything.
    79         *
    80         *  @field(newFileMode) the access permissions of the output file.
    81         *      Normally the file will have the access permissions that exist at
    82         *      the time archive is created.  However, there may be times when
    83         *      the developer wants/needs to make a file readonly that is (for
    84         *      development purposes) writable.  Only two modes are supported "r"
    85         *      (readonly) and "rw" (readable and writable).
    86         *
    87         *  @see #filterMap
    88         */
    89        struct Filter {
    90            any         operation;      /*! the JavaScript function to run */
    91            any         args[];         /*! additional arguments for operation */
    92            String      newFileName;    /*! the new file name */
    93            String      newFileMode;    /*! either "r" or "rw" */
    94        }
    95    
    96        /*!
    97         *  ======== compatibilityKey ========
    98         *  The released package's compatibility key
    99         *
   100         *  This string contains the value declared in the package's `package.xdc`
   101         *  specification file.
   102         *
   103         *  @a(readonly)  This value is initialized before the release script or
   104         *                any of its filters are run and should not be modified.
   105         */
   106        config String compatibilityKey;
   107    
   108        /*!
   109         *  ======== buildCount ========
   110         *  A unique build count for the released package.
   111         *
   112         *  This string contains is a decimal number that increments at least
   113         *  once every time the package is released.  This string together with
   114         *  the compatibility key forms a unique version number for the package.
   115         *
   116         *  @a(readonly)  This value is initialized before the release script or
   117         *                any of its filters are run and should not be modified.
   118         */
   119        config String buildCount;
   120    
   121        /*!
   122         *  ======== packageName ========
   123         *  The released package's name
   124         *
   125         *  This string contains the value declared in the package's `package.xdc`
   126         *  specification file.
   127         *
   128         *  @a(readonly)  This value is initialized before the release script or
   129         *                any of its filters are run and should not be modified.
   130         */
   131        config String packageName;
   132        
   133        /*!
   134         *  ======== releaseName ========
   135         *  The release's name
   136         *
   137         *  This string contains the value declared in the package's `package.bld`
   138         *  build script; it is the name of the output archive without the
   139         *  "`.tar`" extension.
   140         *
   141         *  @a(readonly)  This value is initialized before the release script or
   142         *                any of its filters are run and should not be modified.
   143         */
   144        config String releaseName;
   145        
   146        /*!
   147         *  ======== files ========
   148         *  An array of files in the release
   149         *
   150         *  The file names in this array include the package's name; i.e.,
   151         *  these names are relative to the package's repository rather than 
   152         *  the package's build directory.
   153         *
   154         *  This value is initialized before the release script or any of its
   155         *  filters are run, and it contains the the names of the files specified
   156         *  directly or indirectly by the package's build script.
   157         *
   158         *  By default, this list does not contain all files in this package
   159         *  release, it excludes files that are commonly copied verbatim into
   160         *  the release (see below).  To get the complete list you must call
   161         *  `{@link #getAllFiles Manifest.getAllFiles}`.
   162         *
   163         *  The excluded files are those that are indirectly included either via
   164         *  @p(blist)
   165         *      - a directory named in `{@link PackageContents#otherFiles}` or
   166         *        `{@link Release#otherFiles}`,
   167         *      - a repository added via `{@link PackageContents#addRepository}`,
   168         *        or
   169         *      - the documentation directory named by
   170         *        `{@link PackageContents#docDir}`
   171         *  @p
   172         *
   173         *  It is possible to remove files from a release by removing it from
   174         *  this array; only files in this array or that are in the specified
   175         *  verbatim directories, the directories named above, will appear in
   176         *  the release.  To remove files that are in any of these directories
   177         *  use `{@link #getAllFiles Manifest.getAllFiles}` to re-initialize
   178         *  `files` so that it contains all of the release's files, then
   179         *  selectivly remove the files from this array.
   180         *
   181         *  It is also possible to add files to a release by adding files to
   182         *  this array.  In fact, files added to the release can be generated
   183         *  by the filter operation specified for the file in
   184         *  `{@link #filterMap}`.  However, since these files are only present
   185         *  in releases of a  package (they are not built as part of the normal
   186         *  build of `all` files and only appear in installed releases of a
   187         *  package), packages that must be built as part of building this
   188         *  release should not refer to these files.
   189         */
   190        config String files[];
   191    
   192        /*!
   193         *  ======== filterMap ========
   194         *  A map of filters for each file in the release
   195         *
   196         *  This map is indexed by the name of the file (as it appears in the
   197         *  `{@link #files}` array) in the release and defines for each file a
   198         *  filter that is applied to the file before it is archived in a
   199         *  release.
   200         *
   201         *  @a(example)  The following script fragment illustrates how one can
   202         *  filter all *.c files in a release through a custom JavaScript
   203         *  function named `copyright`.
   204         *      @p(code)
   205         *      function copyright(args, ...) { ...}
   206         *
   207         *      for (var i = 0; i < Manifest.files.length; i++) {
   208         *          var fileName = Manifest.files[i];
   209         *          if (fileName.match(/\.c$/) != null) {
   210         *              Manifest.filterMap[fileName] = {operation: copyright};
   211         *          }
   212         *      }
   213         *      @p
   214         *
   215         *  @see #files
   216         */
   217        config Filter filterMap[string];
   218    
   219        /*!
   220         *  ======== getAllFiles ========
   221         *  Read the entire release manifest into the Manifest.files array
   222         *
   223         *  This function re-reads the release's manifest into the
   224         *  `Manifest.files` array but only excludes the directories whose
   225         *  names appear in the `String` array `verbatimDirs`.  
   226         *
   227         *  @param(verbatimDirs)    array of strings naming directories relative
   228         *                          to the package's base directory.  Each
   229         *                          directory named in this array (and all the
   230         *                          files and sub-directories it contains) is 
   231         *                          excluded from the `Manifest.files` array and 
   232         *                          is automatically added to the release without
   233         *                          change.
   234         *
   235         *                          If this array is `null` or empty, all files
   236         *                          in the release are read into the
   237         *                          `Manifest.files` array.
   238         */
   239        Void getAllFiles(String verbatimDirs[]);
   240    }
   241    /*
   242     *  @(#) xdc.bld; 1, 0, 2,297; 11-16-2010 11:20:04; /db/ztree/library/trees/xdc/xdc-v53x/src/packages/
   243     */
   244