1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== Library.xdc ========
    14     */
    15    package xdc.bld;
    16    
    17    /*!
    18     *  ======== Library ========
    19     *  Model of a searchable collection of object files
    20     *
    21     *  A library is a collection of one or more object files that is searched
    22     *  to resolve undefined references at link time.
    23     *
    24     *  Instances of this module represent a target independent collection of
    25     *  object files that implement a single set of APIs.  Thus, a library is
    26     *  really a container of target-specific archives which contain the object
    27     *  files necessary to implement a common API.  Although, a library may
    28     *  contain target dependent APIs, each library is expected to
    29     *  encapsulate the same basic functionality independent of the target.
    30     *
    31     *  Instances must be created via the
    32     *  `{@link xdc.bld.PackageContents#addLibrary()}` function; this
    33     *  ensures that each library created appears in the package's manifest and
    34     *  that it properly "inherits" appropriate default attributes from the
    35     *  containing package.
    36     *
    37     *  Library instances are initially create without *any* objects; this ensures
    38     *  that the developer complete control over what objects should be in each
    39     *  library. Thus, even modules declared in a package's specification,
    40     *  `package.xdc`, must be explicitly added to each library in the package
    41     *  (via `{@link #addObjects()}`).
    42     */
    43    metaonly module Library {
    44        /*!
    45         *  ======== Attrs ========
    46         *  Optional attributes for a Library instance.
    47         *
    48         *  Unspecified attributes are "inherited" from
    49         *  `{@link xdc.bld.PackageContents#Attrs}`; i.e., if one of fields in this
    50         *  structure is unspecified *and* this field's name matches a field name
    51         *  in `{@link xdc.bld.PackageContents#attrs}`, then this field's value
    52         *  defaults to the value in specified by
    53         *  `{@link xdc.bld.PackageContents#attrs}`.  This mechanism makes it
    54         *  possible to establish package-wide default values for any of the
    55         *  "inherited" attributes.
    56         *
    57         *  Suppose, for example, that you want all archives in this
    58         *  package to be build with the '`release`' profile, but one particular 
    59         *  archive must be built with '`debug`' (because it is a source example).
    60         *  The following build script fragment shows how this can be
    61         *  accomplished:
    62         *  @p(code)
    63         *      Pkg.attrs.profile = 'release';
    64         *      var lib = Pkg.addLibrary('example', ..., {profile: 'debug'});
    65         *  @p
    66         *  @field(incs)  This string contains include path options used by
    67         *          the compiler (or assembler) to locate include files; e.g.,
    68         *          "`-I ../../include -I ../c55xx`".  Note that the syntax of 
    69         *          this string may be target dependent.
    70         *
    71         *  @field(defs)  This string contains options used by the
    72         *          compiler (or assembler) to define macros; e.g.,
    73         *          "`-D_C6xxx -DDEBUG=1`".  Note that the syntax of 
    74         *          this string may be target dependent.
    75         *
    76         *  @field(aopts)  This string contains options used by the assembler
    77         *          to produce object files; e.g., "`-mP1`".  Note that the syntax
    78         *          of this string may be target dependent.
    79         *
    80         *  @field(copts)  This string contains options used by the C/C++
    81         *          compiler to produce object files; e.g., "`-o3 -mi1`".  Note
    82         *          that the syntax of this string may be target dependent.
    83         *
    84         *  @field(aropts)  This string contains options used by the archiver
    85         *          produce archive files; e.g., "`-q`".  Note
    86         *          that the syntax of this string may be target dependent.
    87         *
    88         *  @field(exportSrc)  If this field is set to true, the sources
    89         *          specified via `{@link #addObjects}()`
    90         *          will be part of the releases named in the releases
    91         *          array.  If it is unspecified (or set to `null`) and the
    92         *          release specifies that sources are to be exported,
    93         *          the sources will be part of the release.  In
    94         *          all other cases, the sources are not part of the
    95         *          release.
    96         *
    97         *  @field(suffix)  If this string is set to a non-`null` value, it 
    98         *          specifies the suffix (or extension) of the archive produced.
    99         *          This suffix is used in lieu of the default suffix
   100         *          ("`.a<targ_suffix>`", where `<targ_suffix>` is the suffix
   101         *          property of the target used to create the archive).  So,
   102         *          care must be taken when creating multiple libraries for
   103         *          different targets to ensure that the resulting archive names
   104         *          are unique.
   105         *
   106         *  @field(profile)  This string names a profile defined by the
   107         *          library's target.  The profile specifies a set of compiler,
   108         *          assembler, and archiver options that are to be used when 
   109         *          producing the archive.  Note that these tool options are
   110         *          in addition to any options specified via `aopts`, `copts`,
   111         *          etc.
   112         *
   113         *  @field(releases)  This array contains releases that will contain the
   114         *          library.  Thus, a single library can be part of any set of
   115         *          releases.  Each library is always added to the package's
   116         *          "default release" in addition to any releases specified in
   117         *          the releases array.
   118         *
   119         *  @see #attrs
   120         *  @see xdc.bld.PackageContents#Attrs
   121         */
   122        struct Attrs {
   123            String  profile;    /*! target options profile */
   124            String  aopts;      /*! asm options for objects */
   125            String  copts;      /*! C/C++ options for objects */
   126            String  defs;       /*! definitions for added objects */
   127            String  incs;       /*! include options for objects */
   128            String  aropts;     /*! library-specific archiver options */
   129            String  suffix;     /*! optional suffix of library name; e.g.,".lib" */
   130            Bool    exportSrc;  /*! if true, export library sources to releases */
   131            Release.Instance releases[];  /*! releases this library is a part of */
   132        };
   133    
   134    instance:
   135        /*!
   136         *  ======== create ========
   137         *  @_nodoc
   138         *  Instances should only be created via PackageContents.addLibrary()
   139         */
   140        create();
   141    
   142        /*!
   143         *  ======== name ========
   144         *  The base name of the library.
   145         *
   146         *  This name names a sub-directory in the package directory that
   147         *  contains all the object files and archives created for each of the
   148         *  targets specified.
   149         *
   150         *  The name of each library is `<name>/<name>.a<target_suffix>`, where
   151         *  `<name>` is the base name and `<target_suffix>` is the suffix property
   152         *  of the target for which the library is built.  For example, one is
   153         *  building a `"hello"` library for big endian C62 the library's file
   154         *  name is "`hello/hello.a62e`"
   155         */
   156        config String name;
   157    
   158        /*!
   159         *  ======== target ========
   160         *  The target used to build objects added to this library.
   161         */
   162        config ITarget.Module target;
   163    
   164        /*!
   165         *  ======== attrs ========
   166         *  This library's optional attributes.
   167         *
   168         *  These attributes are "inherited" by all objects added to this
   169         *  library; i.e., any object attribute that is undefined but is
   170         *  defined here will be assigned the value from these attributes.
   171         *
   172         *  Similarly, any unspecified attributes that also appear in
   173         *  `{@link xdc.bld.PackageContents#Attrs}` are inherited from
   174         *  `{@link xdc.bld.PackageContents#attrs}`.
   175         *
   176         *  @see xdc.bld.PackageContents#Attrs
   177         */
   178        config Library.Attrs attrs;
   179        
   180        /*!
   181         *  ======== addObjects ========
   182         *  Add specified object to be built and archived into this library.
   183         *
   184         *  Examples
   185         *
   186         *      1. Locate a source file whose name starts with "fir" with
   187         *      an extension supported by the library's target, compile it
   188         *      and add to the library lib:
   189         *      @p(code)
   190         *          lib.addObjects(["fir"]);
   191         *      @p
   192         *      If fir.c exists compile and add to lib, if fir.asm exists
   193         *      assemble and add to lib, etc.  If no such file is located,
   194         *      an warning is emitted.
   195         *
   196         *      2. Compile `fir.c` and `iir.c` and add to the library `lib`:
   197         *      @p(code)
   198         *          lib.addObjects(["fir.c", "iir.c"]);
   199         *      @p
   200         *      3. Names may include sub-directory prefixes.  In this case, the
   201         *      source will be located in a sub-directory of the current
   202         *      package.  The following statement declares that the file
   203         *      "`foo/fir.c`" should be compiled and added to the library
   204         *      `lib`:
   205         *      @p(code)
   206         *          lib.addObjects(["foo/fir.c"]);
   207         *      @p
   208         *      As in the previous examples, the extension ".c" is optional. 
   209         *      In case an extension is not supplied, each extension
   210         *      understood by the target will be tried until a source file
   211         *      is located.
   212         *
   213         *      4. It is also possible to supply file specific compilation
   214         *      options.
   215         *      @p(code)
   216         *          lib.addObjects(["fir.c", "iir.c"], {defs: "-D_DEBUG"});
   217         *      @p
   218         *      In this case, both files `fir.c` and `iir.c` will be compiled
   219         *      with the "`-D_DEBUG`" flag.  Any setting of `attrs.defs` in the
   220         *      library or package is overridden by this definition.
   221         *
   222         *  @param(names)       array of base names of the sources of object files
   223         *                      to be created and archived into the library.
   224         *                      See NOTE in `{@link xdc.bld}` for filename rules.
   225         *
   226         *  @param(objAttrs)    optional `{@link Object#Attrs}` for the array of
   227         *                      objects added; all objects named by `names` will be
   228         *                      given the attributes `objAttrs`.
   229         *
   230         *  @a(returns)         `void`
   231         *
   232         *  @a(throws)          `Error` exceptions are thrown for fatal errors
   233         *
   234         */
   235        Void addObjects(String names[], Object.Attrs objAttrs = {});
   236    }
   237    /*
   238     *  @(#) xdc.bld; 1, 0, 2,297; 11-16-2010 11:20:04; /db/ztree/library/trees/xdc/xdc-v53x/src/packages/
   239     */
   240