From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - xdc.setCurPkgBase
Set the current package base
Contents |
Synopsis
| xdc.setCurPkgBase(packageBasePath); |
Parameters
- packageBasePath
- string path name of a package's base directory.
Description
xdc.setCurPkgBase can be used to dynamically change the current package.
This will change the package path in the event that the new package is not in the same repository as the previous package base.
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved