From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - xdc.om.Package-Name
A hash table of all loaded packages
Synopsis
| var pkg = xdc.om["«pkg_name»"]; |
Description
As packages are loaded, either directly or indirectly, during the execution of any XDCscript script, xdc.om["«pkg_name»"] is set to the package object that represents the package whose name is "«pkg_name»".
See Also
XDCscript - xdc.loadPackage | Load specified package |
XDCscript - xdc.om | Top-Level object of current domain model |
XDCscript - Package-Object | Object containing package-wide features of a package |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved