From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - Typed-Object.$self
This object
Contents |
Synopsis
| «tobj».$self |
Description
The $self property of a typed object simply returns itself. This is useful for bulk assignment when «tobj» is a JavaScript variable; without this property, assignment of a JavaScript object to «tobj» would simply replace the typed object with the JavaScript object rather than performing a field-by-field assignment to the typed object.
See also
XDCscript - Typed-Object | Objects specified by the RTSC Interface Definition Language |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved