From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - Module-Object.$name
Canonical name of the module
Contents |
Synopsis
| «mod».$name |
where «mod» is a module object.
Description
The $name property of module object is the canonical name of the module. For example, the $name property of the System module in the xdc.runtime package is just "xdc.runtime.System".
See also
XDCscript - Module-Object | Object containing per-module-features of a module |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved