From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
XDCscript - Instance-Object
Object containing per-instance-features of a module
Contents |
Description
Instance objects reflect the per-instance-feature(s) of a module specification. They are created using the module's create method.
See Also
XDCscript_-_Module-Object.create | Create a new Instance object managed by this unit |
XDCscript - Instance-Object.$index | Serial number of the instance |
XDCscript - Instance-Object.$module | The Module object that manages this instance |
XDCscript - Instance-Object.$name | Canonical name for the instance |
XDCscript - Instance-Object.$package | The Package object containing the module managing this instance |
XDCscript - Instance-Object.$private | Private state object of the instance |
XDCscript - Instance-Object.$super | Instance of the inherited-interface |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved