1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Main.xdc ========
15 */
16
17 package xdc.runtime;
18
19 /*!
20 * ======== Main ========
21 * Configuration "stand-in" for application code.
22 *
23 * This module is used to enable "module" configuration of application code
24 * that is not part of a module. Configuration of this `Main` module is
25 * used for all code not in a module.
26 *
27 * For example, an `ILogger` "service provider" for all code that is not in
28 * a RTSC module can be configured by setting this module's `logger`; when
29 * code that is not in a module calls `Log_print()`, for example, this
30 * module's `ILogger` handles the event.
31 *
32 * Since this module is "gated", the user can also assign a gate to this
33 * module for use by any code that is not in a module. This gate can be used
34 * to serialize access to global data by multiple threads in the system.
35 * @p(code) 36 * #include <xdc/runtime/Main.h>
37 * #include <xdc/runtime/Gate.h>
38 * :
39 * int global = 0;
40 * int main() {
41 * : // create a bunch of threads
42 * }
43 *
44 * void thread() {
45 * IArg key = Gate_enterModule(); // enter critical section
46 * global++; // safely update global data
47 * Gate_leaveModule(key); // leave critical section
48 * }
49 * @p 50 */
51 @Gated module Main {
52
53 };
54
55 /*
56 * @(#) xdc.runtime; 2, 1, 0,292; 9-14-2010 16:36:40; /db/ztree/library/trees/xdc/xdc-v49x/src/packages/
57 */
58