From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
XDCscript - Typed-Object.$seal
Seal a typed object or one of its fields
Contents |
Synopsis
| «tobj».$seal(«fieldName») |
Description
Renders the specified field within «tobj» read-only. If «fieldName» is omitted, the entire object is made read-only.
See also
XDCscript - Typed-Object | Objects specified by the RTSC Interface Definition Language |
XDCscript - Typed-Object.$sealed | Test a typed object or one of its fields for being read-only |
XDCscript - Typed-Object.$unseal | Unseal a typed object or one of its fields |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved