From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 04-Aug-2010 21:08 UTC

XDCscript - Instance-Object.$super

Instance of the inherited-interface

Contents

Synopsis

 
«inst».$super

where «inst» is an instance object.

Description

The $super property of an instance object is a Instance object of the Instance type designated in the inherited-interface for the module managing this instance, or null if not specified.

See also

XDCscript - Instance-Object Object containing per-instance-features of a module

[printable version]  [offline version]offline version generated on 04-Aug-2010 21:08 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference