From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
XDCscript - Instance-Body.instance$meta$init
Initialize a meta-only module's instance
Contents |
Synopsis
| function instance$meta$init([r1, ...]) |
Parameters
- r1, ...
- the arguments declared in the module's create method.
Description
This function is invoked whenever a meta-only module's instance create() is called. Configuration model data can be changed as a function of the arguments passed to create().
In instance$meta$init, this is a reference to a structure containing instance configuration parameters.
For information about the order in which module and instance functions are invoked, see Creating Configurable Content.
See also
XDCscript - Instance-Body.instance$static$init | Statically initialize a target module's instance object |
Creating Configurable Content | How to leverage the configuration process |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved