From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Demo of DSPBIOS 5.x Project Creation in CCSv4
Using CCStudio v4 to create a DSP/BIOS 5.x project
This Flash demo shows how to create a CCSv4 project that uses DSP/BIOS 5.x.
When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions.
If you don't see the demo, you can download the Flash player, or save the demo to disk.
See also
Demo of Target Configuration Creation in CCSv4 | Using CCStudio v4 to create a target configuration for debugging |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved