From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Command - xdc.tools.path
Package path display tool
Contents |
Synopsis
| xs xdc.tools.path [options ...] |
For a complete description of this tool's options, see its Cdoc reference page xdc.tools.path.
Description
The path tool displays the packages located along the specified package path. Both textual and graphical versions of this tool are provided. The textual tool is xdc.tools.path and the graphical tool is xdc.tools.path.sg.
By default, the path tool displays a list of all packages found in the repositories referenced by the package path.
For example, output for the xdc.tools.cdoc.sg package is similar to this:
Package Name: xdc.tools.cdoc.sg Repository: C:\xdc_2_94_01\packages Release Name: xdc_tools_cdoc_sg Label: default Compatibility Key: 1, 0, 0, 62 Date: 04/25/2007 19:07
The following command-line options are available:
- -n
- Display only the names of the packages.
- -p
- Echo only the current package path.
- -d
- Display information about the packages in the specified repository
- only. For example:
xs xdc.tools.path -d C:/CCStudio_v3.3/bios_5_31/packages
See also
Command - xdc.tools.path.sg | Interactive Package Path browser tool |
xdc.tools.path | Client documentation for xdc.tools.path |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved