From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
C - Module setMask
Set a module's diagnostics mask
Contents |
Synopsis
| #include <«pkg»/«Mod».h> Void «Mod»_Module_setMask(Bits16 mask) /* set the value of «Mod»'s diagnostic mask */ |
Description
Every module «Mod» provides a parameterless macro named «Mod»_Module_setMask() that sets the current value of the module's diagnostics mask. If the module «Mod» does not have a mask, this method has no effect.
Since
This method was introduced in XDCtools release 3.15.
See also
C - Module_hasMask | Check for a module diagnostics mask |
C - Module_getMask | Get a module's diagnostics mask |
![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved