From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
C - Module heap
Get a module's heap
Contents |
Synopsis
| #include <«pkg»/«Mod».h> #include <xdc/runtime/IHeap.h> IHeap_Handle «Mod»_Module_heap(void) /* The heap associated with «Mod» */ |
Description
Every module «Mod» provide a parameterless macro named «Mod»_Module_heap() that returns the module's statically configured heap handle. This handle, although potentially equal to NULL, may always be passed to the xdc.runtime.Memory functions that require an IHeap instance handle.
Since
This method was introduced in XDCtools release 3.15.
See also
xdc.runtime.IHeap | Client documentation for xdc.runtime.IHeap |
xdc.runtime.Memory | Client documentation for xdc.runtime.Memory |
C - Object_heap | Get a module's instance heap |
[printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved