1 2 3 4 5 6 7 8
9
10 requires xdc.tools.configuro;
11
12 /*!
13 * ======== xdc.tools.configuro.ccs ========
14 * Command-line configuration tool adapter for Code Composer Studio
15 *
16 * @a(INSTALLING_ON_WINDOWS)
17 *
18 * The XDC interface to Code Composer Studio requires some Windows registry
19 * entries for correct operation. By default the XDC product Windows installer
20 * takes care of this transparently to the user. You need only read this
21 * section if you have installed or upgraded the XDC product on Windows without
22 * having used the installer, for example if you are accessing XDC from a
23 * shared network drive.
24 *
25 * To update the required registry entries, do the following steps:
26 * @p(nlist)
27 * - open a Windows command window, for example by typing `cmd` from the
28 * "Run..." menu item located in the Windows "Start" menu.
29 * - type `cd %XDCROOT%`
30 * - type `cd packages\xdc\tools\configuro\ccs`
31 * - type `regsvr32 btiXdc`
32 * - click OK on the dialog box:
33 * @p
34 * @p(html)
35 * <div style="text-align: center;">
36 * <img src="./doc-files/RegSvr32.png"/>
37 * </div>
38 * @p
39 *
40 * If you have not installed XDC using the installer, it is possible that you
41 * also do not have an `%XDCROOT%` environment variable. In this case in step
42 * 2 above, cd to your own XDC product installation directory.
43 */
44 package xdc.tools.configuro.ccs [1, 0, 0, 0] {
45 module Main;
46 }
47 48 49
50