From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 04-Aug-2010 21:08 UTC | ![]() |
C - Instance finalize
Module's instance finalization function
Contents |
Synopsis
| #include "package/internal/«Mod».xdc.h" Void «Mod»_Instance_finalize(«Mod»_Object *obj) /* non-@InstanceInitError modules only */ Void «Mod»_Instance_finalize(«Mod»_Object *obj, Int state) /* @InstanceInitError modules only */ |
Description
Modules that support instances and are specified with the @InstanceFinalize attribute must implement this function, where «Mod» is the name of the module. The type signature of this function depends on whether (or not) «Mod» has the @InstanceInitError attribute. If «Mod» is declared with @InstanceInitError, this function is passed a second integer parameter, state. The state parameter's value is either the return value from a failed «Mod»_Instance_init() call or 0 (in the case of a normal instance delete, for example).
See also
C - delete | Finalize and free this previously allocated instance object |
C - destruct | Finalize the instance object inside the provided structure |
C - Instance_init | Module's instance initialization function |