1 /*
2 *Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12
13 package xdc.tools.repoman;
14
15 /*!
16 * ======== xdc.tools.repoman.Main ========
17 * Repository Manager tool
18 *
19 * This tool creates and manages package repositories. It displays
20 * information about archived packages, extracts archived packages,
21 * extracts repositories from bundles and deletes packages from
22 * repositories.
23 *
24 * Information about archived packages can be displayed with
25 * the '-t' and '-n' options. The '-p' argument is used to
26 * specify a directory in which to search. If the '-p' arg is omitted,
27 * the current directory is searched. Specific packages can searched
28 * for by specifying one or more package names, or one or more package
29 * archives at the end of the command line. If no packages are specified,
30 * information on all packages found in the search directory will be
31 * displayed.
32 *
33 * Archived packages can be extracted to a repository with the '-x'
34 * option. '-x -D' will extract dependent packages, too. '-x -R' will
35 * recursively extract dependent packages. If any of the packages in
36 * the specified package list are not compatible, the operation will
37 * be aborted. '-F' can be used to force all packages to be extracted,
38 * regardles of compatibility. The '-p' arg is used to specify a
39 * directory to search in. If not specified, the current directory will
40 * be searched. The '-x' option also extracts a repository or packages
41 * from a bundle. In this case, the last argument specifies the bundle
42 * from which to extract the repository. The repository to be extracted
43 * is specified with the '-b' arg. If just packages are to be extracted,
44 * one or more package names should follow the name of the repository
45 * that they should be extracted from.
46 *
47 * Packages can be deleted from a repository with '-d'. If the package
48 * has any subdirectores that contain packages, they will be left intact.
49 * After the package is deleted, if the package has no subdirectories
50 * with packages, empty directories that are part of the fully qualified
51 * package will be deleted, too.
52 *
53 * Packages can be copied between repositories with '-c'. If the package
54 * being copied already exists in the destination repository, it will be
55 * deleted prior to being replaced.
56 *
57 * The '-r' argument specifies a destination repository. If '-r' is
58 * omitted, the repository of the current package is used. If there is
59 * no current package, the current directory is used.
60 *
61 * When a package name is given, it can be specified in full, such as
62 * 'ti.platforms.sim6xxx', or the wildcard characters '*' and '?' may be
63 * used, as in 'ti.platforms.*' or 'ti.catalog.c??00'. A version/key can
64 * also be attached to a package name in the following manner:
65 * 'ti.platforms.c6000[1,0,0,0,313835]'. A prefix of the full version/key
66 * may also be used: 'ti.platforms.c6000[1,0]'.
67 *
68 * If a package name has multiple matches either with or without a
69 * version/key specified, the most recent will be selected. Wildcards may
70 * also be used when naming a package archive file.
71 *
72 * @a(Examples) 73 * xs xdc.tools.repoman -t
74 * @p(dlist) 75 * Displays all info on all archived packages in the current directory
76 * @p 77 *
78 * xs xdc.tools.repoman -t -p C:\xdc-o19\exports
79 * @p(dlist) 80 * Displays all info on all archived packages in C:\xdc-o19\exports
81 * @p 82 *
83 * xs xdc.tools.repoman -t -p C:\xdc-o19\exports ti.platforms.*
84 * @p(dlist) 85 * Displays all info on archived packages whose names begin with
86 * ti.platforms. in C:\xdc-o19\exports
87 * @p 88 *
89 * xs xdc.tools.repoman -t -p C:\xdc-o19\exports ti_platforms*.tar
90 * @p(dlist) 91 * Displays all info on packages in files that match ti_platforms*.tar
92 * in C:\xdc-o19\exports
93 * @p 94 *
95 * xs xdc.tools.repoman -t -p C:\xdc-o19\exports ti.catalog.c6000 ti.catalog.sim6xxx
96 * @p(dlist) 97 * Displays all info on archived packages ti.catalog.c6000 and
98 * ti.catalog.sim6xxx in C:\xdc-o19\exports
99 * @p 100 *
101 * xs xdc.tools.repoman -t http://www.sanb.design.ti.com/ti_sdo_ce_wizards_genserver.tar
102 * @p(dlist) 103 * Displays all info on archived package ti_sdo_ce_wizards_genserver.tar
104 * at URL http://www.sanb.design.ti.com
105 * @p 106 *
107 * xs xdc.tools.repoman -x
108 * @p(dlist) 109 * Extracts all archived packages in the current directory to the current
110 * repository
111 * @p 112 *
113 * xs xdc.tools.repoman -x -r C:\myrepo\packages -p C:\exports
114 * @p(dlist) 115 * Extracts all archived packages in C:\exports to C:\myrepo\packages
116 * repository
117 * @p 118 *
119 * xs xdc.tools.repoman -x -r C:\myrepo\packages -p C:\exports ti.catalog.*
120 * @p(dlist) 121 * Extracts packages matching ti.catalog.* from c:\exports to
122 * c:\myrepo\packages
123 * @p 124 *
125 * xs xdc.tools.repoman -x -r C:\myrepo\packages C:\exports\ti_catalog*.tar
126 * @p(dlist) 127 * Extracts packages from files matching C:\exports\ti_catalog*.tar
128 * to c:\myrepo\packages
129 * @p 130 *
131 * xs xdc.tools.repoman -x -r C:\myrepo\packages C:\exports\ti_catalog*.tar
132 * @p(dlist) 133 * Extracts packages from files matching C:\exports\ti_catalog*.tar
134 * to c:\myrepo\packages
135 * @p 136 *
137 * xs xdc.tools.repoman -x -R -r C:\myrepo -p C:\xdc-o19\exports ti.platforms.sim6xxx
138 * @p(dlist) 139 * Extracts the package ti.platforms.sim6xxx and all recursively
140 * dependent packages from C:\xdc-o19\exports to C:\myrepo
141 * @p 142 *
143 * xs xdc.tools.repoman -x -r C:\ -b packages C:\exports\xdc_core.tar.gz
144 * @p(dlist) 145 * Extracts the repository 'packages' from bundle
146 * C:\exports\xdc_core.tar.gz to C:\
147 * @p 148 *
149 * xs xdc.tools.repoman -x -r C:\myrepo -b examples ti.xdais.dm.examples.videnc1_copy
150 * C:\xdais_6_24.tar.gz
151 * @p(dlist) 152 * Extracts the package ti.xdais.dm.examples.videnc1_copy from repository
153 * 'examples' in bundle
154 * C:\xdais_6_24.tar.gz to C:\myrepo
155 * @p 156 *
157 * xs xdc.tools.repoman -x -r C:\myrepo http://www.sanb.design.ti.com/ti_sdo_ce_wizards_genserver.tar
158 * @p(dlist) 159 * Extracts package ti_sdo_ce_wizards_genserver.tar at URL http://www.sanb.design.ti.com
160 * to c:\myrepo
161 * @p 162 *
163 * xs xdc.tools.repoman -r C:\myrepo -b examples
164 * https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/xdais/7_10/exports/xdais_7_10.tar.gz
165 * @p(dlist) 166 * Extracts all of the packages in repository 'examples' from bundle xdais_7_10.tar.gz at URL
167 * http://... to C:\myrepo
168 * @p 169 *
170 * xs xdc.tools.repoman -x -r C:\myrepo -b examples ti.xdais.dm.examples.videnc1_copy
171 * https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/xdais/6_24/exports/xdais_6_24.tar.gz
172 * @p(dlist) 173 * Extracts the package ti.xdais.dm.examples.videnc1_copy in repository
174 * 'examples' from bundle xdais_7_10.tar.gz at URL http://... to C:\myrepo
175 * @p 176 *
177 * xs xdc.tools.repoman -c -r C:\destdir\packages -p C:\srcdir\packages ti.catalog.c6000
178 * @p(dlist) 179 * Copies the package ti.catalog.c6000 from C:\srcdir\packages to
180 * C:\destdir\packages
181 * @p 182 *
183 * xs xdc.tools.repoman --rsave -f c:/repoinfo.rmn -p c:/pkgarchives;c:/testpkgs c:/myrepo
184 * @p(dlist) 185 * Saves package information for repository c:/myrepo to file c:/repoinfo.rmn.
186 * Also saves the search path c:/pkgarchives;c:/testpkgs
187 * @p 188 *
189 * xs xdc.tools.repoman --rrestore -f c:/repoinfo.rmn -p c:/pkgarchives;c:/testpkgs
190 * @p(dlist) 191 * Restores all of the packages in the repository referenced in
192 * c:/repoinfo.rmn. Uses the search path c:/pkgarchives;c:/testpkgs to find
193 * and copy packages. Will create the repository if it doesn't exist.
194 * @p 195 *
196 * xs xdc.tools.repoman --rcreate -f c:/repoinfo.rmn -p
197 * c:/pkgarchives;c:/testpkgs c:/mynewrepo
198 * @p(dlist) 199 * Creates the new repository c:/mynewrepo from the repository referenced in
200 * the file c:/repoinfo.rmn. Uses the search path c:/pkgarchives;c:/testpkgs
201 * to find and copy packages. If successful, the newly created repository
202 * will be identical to its predecessor referenced in c:/repoinfo.rmn.
203 * @p 204 *
205 * xs xdc.tools.repoman --providerId my_codec_engine c:/codec_engine_2_23/mypackages
206 * @p(dlist) 207 * Assigns the providerId attribute in c:/codec_engine_2_23/mypackages/.repo.xml
208 * the value my_codec_engine. If c:/codec_engine_2_23/mypackages/.repo.xml does not
209 * exist, it will be created.
210 * @p 211 *
212 */
213 metaonlymodule Main inherits xdc.tools.ICmd {
214
215 overrideconfig String usage[] = [
216 '-t [-v] [-p pathname] [packagename...|packagefile...]',
217 '-n [-v] [-p pathname] [packagename...|packagefile...]',
218 '-x [-v] [-D] [-R] [-F] [-r destrepo] [-p path] packagename...|packagefile...',
219 '-x [-v] [-D] [-R] [-F] [-r destrepo] [-p path] -b bundlerepository [packagename...] bundleFile',
220 '-d [-v] [-F] [-r destrepo] packagename...',
221 '-c [-v] [-F] [--providerId] [-r destrepo] [-p pathname] packagename...',
222 '--rsave -f file [-p searchpath] repository...',
223 '--rrestore -f file [-p searchpath] [index-spec]',
224 '--rcreate -f file [-p searchpath] [index-spec] destrepository...',
225 '[-F] --providerId providerId [repository...]'
226 ];
227
228 /*! represents a repository in a bundle */
229 @XmlDtd
230 metaonlystruct Repo {
231 String name;
232 String pkg[];
233 }
234
235 @XmlDtd
236 metaonlystruct Pkg {
237 String name;
238 String file;
239 String release;
240 String label;
241 String version;
242 String date;
243 String buildable;
244 String originalProviderId;
245 String producerId;
246 String reqs[];
247 String refs[];
248 Repo repository[];
249 }
250
251 @XmlDtd
252 metaonlystruct Results {
253 String repository;
254 String providerId;
255 String producerId;
256 Bool writable;
257 Pkg pkg[]; /*! array of package info structures */
258 }
259
260 @XmlDtd
261 metaonlystruct PkgName {
262 String name;
263 Repo repository[];
264 }
265
266 @XmlDtd
267 metaonlystruct NameResults {
268 PkgName pkgName[]; /*! array of PkgName structures */
269 }
270
271 instance:
272
273 //!Display package info
274 @CommandOption('t')
275 config Bool infoFlag = false;
276
277 //!Display package names only
278 @CommandOption('n')
279 config Bool namesFlag = false;
280
281 //!Extract package(s)
282 @CommandOption('x')
283 config Bool extractFlag = false;
284
285 //!Delete package(s)
286 @CommandOption('d')
287 config Bool deleteFlag = false;
288
289 //!Path arg
290 @CommandOption('p')
291 config String pathArg = null;
292
293 //!Repository arg
294 @CommandOption('r')
295 config String repositoryArg = null;
296
297 //!Include package dependencies
298 @CommandOption('D')
299 config Bool dependentFlag = false;
300
301 //!Recursive include package dependencies
302 @CommandOption('R')
303 config Bool recursiveDepFlag = false;
304
305 //!Return an array of strings
306 @CommandOption('a')
307 config Bool arrFlag = false;
308
309 //!Return a Results struct as XML
310 @CommandOption('X')
311 config Bool xmlFlag = false;
312
313 //!Print informative messages during execution
314 @CommandOption('v')
315 config Bool verboseFlag = false;
316
317 //!Bundle repository arg
318 @CommandOption('b')
319 config String bundleRepositoryArg = null;
320
321 //!Force incompatible packages
322 @CommandOption('F')
323 config Bool forceFlag = false;
324
325 //!Copy package(s)
326 @CommandOption('c')
327 config Bool copyFlag = false;
328
329 //!file arg to save/restore repository
330 @CommandOption('f')
331 config String fileArg = null;
332
333 //!Save a repository's information to file
334 @CommandOption('rsave')
335 config Bool rsaveFlag = false;
336
337 //!Restore one or more repositories from information in file
338 @CommandOption('rrestore')
339 config Bool rrestoreFlag = false;
340
341 //!Create one or more repositories from information in file
342 @CommandOption('rcreate')
343 config Bool rcreateFlag = false;
344
345 //! providerId for a repository
346 @CommandOption('providerId')
347 config string provIdArg = null;
348
349 }
350
351
352
353 /*
354 * @(#) xdc.tools.repoman; 1, 0, 0,184; 8-4-2010 15:09:53; /db/ztree/library/trees/xdctools/xdctools-d42x/src/
355 */
356