From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |
XDCspec - @DirectCall
Always generate a direct call to this function
Contents |
Synopsis
| @DirectCall |
Description
Methods with the DirectCall attribute do not call through a function stub generated at configuration time. This attribute ensures that there is no extra overhead for call to this method even in unoptimized builds of an application. However, it also means that this method can not be traced via implicit logging.
See also
Using_xdc.runtime_Logging/Example_2 | Events provided by all RTSC target modules |
[printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved