From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - xdc.om
Top-Level object of current domain model
Contents |
Description
Every script executes in the domain of some "object model". Each model has a set of global objects that are appropriate for scripts executing within the model. For example, configuration scripts (*.cfg) execute in the configuration model and can freely reference the global Program object to read or set properties of the the current program. Similarly, build scripts (package.bld and config.bld) execute in the build model and can access the global Build and Pkg objects.
The properties of the xdc.om can be used by scripts to reflect on the current model. For example, the xdc.om.$name property can be used to distinguish between the configuration model and the build model.
See Also
XDCscript - xdc.om.$curpkg | A model-specific current package |
XDCscript - xdc.om.$homepkg | A model-specific home package |
XDCscript - xdc.om.$modules | Array of all modules in the current model |
XDCscript - xdc.om.$name | Model name |
XDCscript - xdc.om.$packages | Array of all packages within the current model |
XDCscript - xdc.om.$root | A model-specific root object |
XDCscript - xdc.om.Package-Name | A hash table of all loaded packages |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved