From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Vector-Object.$add
Append element to the end of a vector
Contents |
Synopsis
| «vec».$add(«arg»); |
Description
This method appends an element to the end of a vector and is equivalent to «vec»[«vec».length++] = «arg».
See also
XDCscript - Typed-Object | Objects specified by the RTSC Interface Definition Language |
XDCscript - Vector-Object | A typed JavaScript array |
XDCscript - Vector-Object.length | Get or set the number of values in a vector |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved