From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Module-Object.Params
Module's instance creation parameters
Contents |
Synopsis
| var «params» = new «Mod».Params(); |
Description
For a module «Mod» that manage instances, «Mod».Params is a constructor that is used to create a "structure" that contains fields for each instance configuration parameter declared by «Mod». Thhis structure is used to create new instance managed by «Mod».
In addition to the configuration parameters declared by «Mod», «Mod».Params also contains a special field, named instance, which defines instance creation parameters common to all modules and is declared by xdc.runtime.IInstance.
Example
| var LoggerBuf = xdc.useModule("xdc.runtime.LoggerBuf"); /* create and initialize a LoggerBuf Params object */ var params = new LoggerBuf.Params(); params.numEntries = 128; params.instance.name = "myLogger"; /* create new LoggerBuf instance object */ ... = Logger.create(params); |
See also
XDCscript - Module-Object.create | Create a new Instance object managed by this unit |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved