From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Module-Object.Function-Name
Module method
Contents |
Synopsis
| «Mod».«methodName» |
where «Mod» is an module object and «methodName» is the name of a method whose type signature is specified in a function-declaration.
Description
Methods of a module object are module-specific properties declared in the module's .xdc specification file. Only methods declared to be metaonly (directly or indirectly) can invoked from scripts; all other method name simply represent the type signature of a function that can be invoked on the target.
Meta-only methods are functions that can be directly invoked from scripts. For example, a module method getName of the module pkg.Mod can be run from a script as shown below.
| var Mod = xdc.module("pkg.Mod"); /* get the module */ print(Mod.getName()); /* run a module method and print result */ |
Meta-only methods have a distinguished function property named $apply that allows them to be invoked with a user specified this pointer. This can be useful when a method needs to invoke the meta-only method associated with an inherited interface. Suppose for example that the pkg1.Mod module inherits from the interface pkg2.IMod. If pkg2.IMod declares and implements a method, say getName, the module pkg1.Mod can both override the implementation provided by pkg2.IMod and invoke the overridden method.
Mod.xs | |
| function getName() { var sup = this.$super.getName.$apply(this, []); /* get inherited name */ return (sup+ ":Mod"); /* return "super_name:my_name" */ } |
The $apply() function has the same signature and semantics as the JavaScript apply() method of Functions.
See also
XDCscript - Module-Object | Object containing per-module-features of a module |
XDCscript - Module-Object.$super | The interface from which this module inherits |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |