From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Module-Body.module$static$init
Initialize module's State object
Contents |
Synopsis
| function module$static$init(state, mod) |
Parameters
- state
- a typed object that corresponds to the Module_State declaration
- mod
- a typed object representing the current module, containing the values of all module-wide configuration parameters
Description
This method initializes the module's state object (declared in by Module_State in the module's specification) based on module-wide configuration parameters.
The values used to initialize state are used to initialize the corresponding target-side module static data. No changes to configuration parameters are allowed here.
See also
XDCscript - Module-Body.module$meta$init | Initialize meta-domain module state |
Creating Configurable Content | How to leverage the configuration process |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved