From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Instance-Object.$private
Private state object of the instance
Contents |
Synopsis
| «inst».$private |
where «inst» is an instance object.
Description
The $private property of an instance object is an untyped JavaScript object that is used by the module's XDCscript methods to maintain state associated with the instance.
See also
XDCscript - Module-Body | The implementation of a module |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved