From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |
Using Encoded Types
How to create and use encoded types
TODO: belongs in the XDCtools User's Guide as a "WHATIS" + "HOWTO"
Contents |
Introduction
RTSC modules have a dual existence: they exist in the meta-domain and (optionally) in the target-domain. On the other hand, modules have a single specification file. So, by default, a single specification results in the generation of two bindings: one for the meta-domain and one for the target domain. In most cases, the representation of types declared in the module's specification have an obvious representation in the target-domain.
However, there are situations where the module producer wants the target-domain representation of a type to differ from the default target-domain representation. For example, you need the representation of a target type to be a single integer whereas in the meta-domain (where there are virtually no performance constraints) the type is a multi-field structure. In these situations, you can declare the type to be "encoded" and take control of the target-domain representation of values having the specified encoded type.
Implementing An Encoded Type
When a type is declared with the @Encoded attribute the module must:
- have custom headers that declare the C type, and
- have a meta-domain file that defines functions that describe the alignment, sizeof and encoding of the type.
Module's Custom C/C++ Header
Module's Custom C/C++ Header. The module's custom headers, Mod__prologue.h and Mod__epilogue.h, must declare the C type for the type declared in the modules specification.
| typedef xdc_Bits32 xdc_runtime_Log_Event; |
Module's Meta-Domain Implementation
Module's Meta-Domain Implementation. The Mod module's meta-domain implementation file, Mod.xs, must define the following three functions for each encoded type EType:
- EType$alignof() - returns an integral target alignment value for the type in MAUs,
- EType$sizeof() - returns an integral target size value for the type in MAUs, and
- EType$encode(desc) - returns a string containing a C expression that evaluates to a constant that represents the value of the meta-domain value desc
| /* * ======== Event$alignof ======== * Return alignment required for an encoded value of an EventDesc */ function Event$alignof() { return (Program.build.target.stdTypes.t_Int32.align); } /* * ======== Event$encode ======== * Return a C expression that evaluates to the encoded value of an EventDesc */ function Event$encode(desc) { var encodedDesc = "0"; if (desc) { encodedDesc = "(((xdc_runtime_Log_Event)" + desc.$private.id + ") << 16 | " + (desc.mask & 0xFFFF) + ")"; } return (encodedDesc); } /* * ======== Event$sizeof ======== * Return sizeof the encoded value of an EventDesc */ function Event$sizeof() { return (Program.build.target.stdTypes.t_Int32.size); } |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |