From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] | offline version generated on 25-Jun-2010 21:06 UTC | ![]() |
ROV Module Writers Guide/Full Examples
Complete examples to test or use as templates
Full Examples
Basic Example
This example demonstrates the most basic features of ROV. Your initial ROV view should be no more complicated than this one.
ModA.xdc | |
| module ModA { metaonly struct BasicView { String label; Int count; Boolean working; }; @Facet metaonly config ViewInfo.Instance rovViewInfo = ViewInfo.create({ viewMap: [ ['Basic', {type: ViewInfo.INSTANCE, viewInitFxn: 'viewInitBasic', structName: 'BasicView'}], ] }); internal: struct Instance_State { UInt16 count; Boolean flag; }; } |
ModA.xs | |
| function viewInitBasic (view, obj) { var Program = xdc.useModule('xdc.rov.Program'); view.label = Program.getShortName(obj.$label); view.count = obj.count; /* Validate count value */ if (obj.count > 3) { Program.displayError(view, "count", "Error: Count should never be larger than 3."); } view.working = obj.flag; } |
Intermediate Example
This example uses ModA from the Basic Example.
ModB.xdc | |
| module ModB { struct Message { UInt16 id; String msg; }; metaonly struct BasicView { String label; String messages[]; Int numSenders; }; @Facet metaonly config ViewInfo.Instance rovViewInfo = ViewInfo.create({ viewMap: [ ['Basic', {type: ViewInfo.INSTANCE, viewInitFxn: 'viewInitBasic', structName: 'BasicView'}] ] }); internal: struct Instance_State { UInt16 numMsgs; Message messages[]; ModA.Handle modAInst; }; } |
ModB.xs | |
| function viewInitBasic (view, obj) { view.label = Program.getShortName(obj.$label); /* Fetch the messages array. */ try { var msgArr = Program.fetchArray(obj.messages$fetchDesc, obj.messages, obj.numMsgs); } catch (e) { Program.displayError(view, "messages", "Error: Problem reading messages array: " + e); return; } /* Fetch the message string from each message */ for each (var msgStruct in msgArr) { try { var message = Program.fetchString(msgStruct.msg); } catch (e) { Program.displayError(view, "messages", "Error: Problem fetching message: " + e); return; } /* Add the message string to the view's messages array. */ view.messages.$add("(" + msgStruct.id + ") " + message); } /* Get the value for numSenders from the ModA handle */ var modAView = Program.scanHandleView('ModA', obj.modAInst); view.numSenders = modAView.count; } |