From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |
High-Level FAQs
General questions about Real-Time Software Components
FAQ-080713-1 | I'm an embedded C programmer, so why should I care about RTSC |
FAQ-080713-2 | What are the essential features/benefits of components in general |
FAQ-080713-3 | How does RTSC expand standard C to embrace software components |
FAQ-080713-5 | What's the relationship between RTSC and the XDCtools product |
FAQ-080713-4 | Can I leverage RTSC with legacy content, or am I starting from scratch |
FAQ-080713-6 | Who's using RTSC today, and what's the roadmap going forward |
FAQ-080713-9 | How is the RTSC-Pedia organized, and what sorts of documents exist |
FAQ-080713-7 | If I'm only consuming RTSC content, what should I read next |
FAQ-080713-8 | I also want to produce RTSC content, what should I read next |