From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() ![]() |
Demo of Customizing Memory Sections
Editing a platform package and defining your own memory sections
The Flash demo below is Part 2 in a series of RTSC Platform Wizard demos that begins with the Demo of the RTSC Platform Wizard in CCSv4. It shows how to further customize the memory sections defined for a platform package. It also shows how to reopen and rebuild a platform package you have created.
When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions.
If you don't see the demo, you can download the Flash player, or save the demo to disk.
RTSC Platform Wizard Demo Part 3: Next, you can continue on to the third demo in this series shows the files in a custom RTSC platform package and the zip file you can use to distribute the package.
See also
Demo of the RTSC Platform Wizard in CCSv4 | Using CCStudio v4 to create a custom RTSC platform |
Demo Showing Files in a Custom Plaform Package | Platform package directory contains zip file for distribution |
Demo Building with Custom Platform Package | Set RTSC configuration project properties and compare a platform to a generated map file |
RTSC+CCStudio v4 QuickStart | Using CCStudio v4 to create, build, and debug RTSC projects |
RTSC+Eclipse FAQs | Using RTSC with Eclipse-Based Tools |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() ![]() |